RTC wakeup pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,378件の閲覧回数
amleng
Contributor IV

Hello,


I need to use RTC wakeup pin(L5) in K60FN1M0VMD12 chip. I couldn't find any support in MQX bsp for using this pin. I wonder if anyone knows how can I configure the chip to enable this pin? Do I need add something in rtc interrupt subroutine regarding this pin?

Cheers!

タグ(3)
0 件の賞賛
返信
1 解決策
1,107件の閲覧回数
Rick_Li
NXP Employee
NXP Employee

Dear amleng,

I'm sorry for delay replying, I just moved your post to this MQX community.

regarding to your issue, I suppose you want use the low power mode of K60 and then wakeup by RTC.

could you please refer to AN4447 which is available at:

https://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MQX&fpsp=1&tab=Documentation_Tab

hope it helps!

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,108件の閲覧回数
Rick_Li
NXP Employee
NXP Employee

Dear amleng,

I'm sorry for delay replying, I just moved your post to this MQX community.

regarding to your issue, I suppose you want use the low power mode of K60 and then wakeup by RTC.

could you please refer to AN4447 which is available at:

https://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MQX&fpsp=1&tab=Documentation_Tab

hope it helps!

0 件の賞賛
返信