I want to communicate over RS485 using TWR- MCF32259 and TWR-SER board .I am using MQX 4.2 and CodeWarrior v11 .I have tried Ethernet to serial example on RS232 my full duplex communication working but As I changes jumper setting for RS 485 I can only transmit data cant receive.There is no RS485 example for TWR-MCF32259 available in MQX4.2
Hi Ajay:
Yes, there is no example on rs485 for MCF32259.
I think you can contact with Embedded Access, the owner of MQX, to see if they have more information for your case
Embedded Access – MQX Design, Products, & Services
Anyway, you can refer to the following thread.
RS485 Flow control on ColdFire 54415
I hope it helps
Regards
Daniel