Problems with Clocking on K70 with MQX 4.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems with Clocking on K70 with MQX 4.1

Jump to solution
2,180 Views
chrissolomon
Contributor III

Hi,

I am trying to get the clocking working for a product using MQX 4.1.0.1.

The product previously worked with MQX 4.0.1. During the upgrade I would like to use a clock setup based on the code from the example BSP for the K70.

 

We have 2 clock modes:

BLPI

MCGOUT = 4MHz sourced from fast internal reference oscillator.

Clock speeds are

Core/System     4MHz

Bus                    4MHz

Flexbus             4MHz

Flash                 1MHz

 

PEE

MCGOUT = 96MHz sourced from 8MHz OSC0 using PLL0

Clock speeds are

Core/System     96MHz

Bus                    48MHz

Flexbus             32MHz

Flash                 16MHz

 

 

On boot the default clock speed is BLPI, then the application switches to PEE when it has verified external supply is available (We can work on battery or external power).

We never switch back to BLPI, if external power is cut we reset.

 

The problem I have is that while I can start the product at either 4MHz or 96MHz, if I attempt to switch to 96MHz from 4MHz I get a reset.

I have tried to debug with GDB with the watchdogs disabled but (possibly as a result of the changing clocks) I get strange behavior (jumps to nonsense addresses, resets for no particular reason etc.)

 

Adding code to make LEDs light up at different phases makes me thing that I am not getting past the transition into FBE.

 

If anyone has any insights, I'd appreciate it!

 

Thanks

 

Chris

Original Attachment has been moved to: bsp_cm.zip

Tags (3)
0 Kudos
Reply
1 Solution
1,881 Views
soledad
NXP Employee
NXP Employee

Hello Chris,

Please check the attached document and let me know if this helps,


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
1,882 Views
soledad
NXP Employee
NXP Employee

Hello Chris,

Please check the attached document and let me know if this helps,


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,881 Views
chrissolomon
Contributor III

Hi Sol,

thanks for the help, with the guidance in the document I was able to generate a new bsp_cm file, and it all seems to work.

Thanks


Chris

0 Kudos
Reply
1,881 Views
chrissolomon
Contributor III

Thanks for the document, it looks interesting, I'll give it a go and post my progress in a day or so.

Chris

0 Kudos
Reply