Ping reply Error 0x1510 in PPP example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Ping reply Error 0x1510 in PPP example

跳至解决方案
1,704 次查看
sumate
Contributor I

Hello All,

 

Now I use TWR-K60N512< TWR-SER> with MQX 3.8 to run a PPP client example <rtcs/examples/shell>.

I have done step by step follow the document ,Everything look fine and connection was established.

But, after that I've never success Ping to any IP, It always reply "Error 0x1510".

Could you please give me a suggestion for this?

 

 

Thank you

...................

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,235 次查看
BryGuyH
Contributor IV

It means no route to host.

 

Its because Freescale hasn't fixed their PPP driver (which also has infinate loops in it as well - so some of your RTCS functions will lock up your code when the ppp link is down).

 

This is what I did to fix the issue:

 

static boolean IPCP_up   (      PPPFSM_CFG_PTR    fsm            /* [IN] - State Machine */   ){ /* Body */   IP_IF_PTR            if_ptr = fsm->PRIVATE;   IPCP_CFG_STRUCT_PTR  ipcp_ptr = if_ptr->HANDLE;   /* Bind the negotiated IP address to this interface */   ipcp_ptr->BIND_PARMS.ihandle = if_ptr;   ipcp_ptr->BIND_PARMS.address = ipcp_ptr->LOPT.ADDR;   ipcp_ptr->BIND_PARMS.network = ipcp_ptr->POPT.ADDR?ipcp_ptr->POPT.ADDR:((ipcp_ptr->LOPT.ADDR & IN_CLASSC_NET) + 1);   //ipcp_ptr->BIND_PARMS.network = ipcp_ptr->POPT.ADDR;   ipcp_ptr->BIND_PARMS.netmask = INADDR_ANY;      RTCSCMD_smartissue(ipcp_ptr->BIND_PARMS, IPIF_bind_ppp);   /* Install a default gateway */   if (ipcp_ptr->INIT.DEFAULT_ROUTE) {      ipcp_ptr->GATE_PARMS.address = ipcp_ptr->POPT.ADDR?ipcp_ptr->POPT.ADDR:((ipcp_ptr->LOPT.ADDR & IN_CLASSC_NET) + 1);      //ipcp_ptr->GATE_PARMS.address = ipcp_ptr->POPT.ADDR;      ipcp_ptr->GATE_PARMS.network = INADDR_ANY;      ipcp_ptr->GATE_PARMS.netmask = INADDR_ANY;      /* Start CR 1133 */      ipcp_ptr->GATE_PARMS.locmask = 0;      /* End CR 1133 */      RTCSCMD_smartissue(ipcp_ptr->GATE_PARMS, IPIF_gate_add);   } /* Endif */#if RTCSCFG_ENABLE_DNS || RTCSCFG_ENABLE_LWDNS   /* Set up the primary DNS server */   if (ipcp_ptr->NEG.NEG_DNS) {#if RTCSCFG_ENABLE_DNS      /* Start CR 2257 */      DNS_SLIST_STRUCT slist_entry;      DNS_init_slist_entry(&slist_entry);      slist_entry.IPADDR = ipcp_ptr->LOPT.DNS;      if (DNS_add_slist_entry(&slist_entry) != DNS_OK)         return FALSE;      /* End CR 2257 */#else      LWDNS_server_ipaddr = ipcp_ptr->LOPT.DNS;#endif   } /* Endif */#endif   if (ipcp_ptr->IP_UP) {      ipcp_ptr->IP_UP(ipcp_ptr->IP_PARAM);   } /* Endif */   return TRUE;} /* Endbody */

 

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,236 次查看
BryGuyH
Contributor IV

It means no route to host.

 

Its because Freescale hasn't fixed their PPP driver (which also has infinate loops in it as well - so some of your RTCS functions will lock up your code when the ppp link is down).

 

This is what I did to fix the issue:

 

static boolean IPCP_up   (      PPPFSM_CFG_PTR    fsm            /* [IN] - State Machine */   ){ /* Body */   IP_IF_PTR            if_ptr = fsm->PRIVATE;   IPCP_CFG_STRUCT_PTR  ipcp_ptr = if_ptr->HANDLE;   /* Bind the negotiated IP address to this interface */   ipcp_ptr->BIND_PARMS.ihandle = if_ptr;   ipcp_ptr->BIND_PARMS.address = ipcp_ptr->LOPT.ADDR;   ipcp_ptr->BIND_PARMS.network = ipcp_ptr->POPT.ADDR?ipcp_ptr->POPT.ADDR:((ipcp_ptr->LOPT.ADDR & IN_CLASSC_NET) + 1);   //ipcp_ptr->BIND_PARMS.network = ipcp_ptr->POPT.ADDR;   ipcp_ptr->BIND_PARMS.netmask = INADDR_ANY;      RTCSCMD_smartissue(ipcp_ptr->BIND_PARMS, IPIF_bind_ppp);   /* Install a default gateway */   if (ipcp_ptr->INIT.DEFAULT_ROUTE) {      ipcp_ptr->GATE_PARMS.address = ipcp_ptr->POPT.ADDR?ipcp_ptr->POPT.ADDR:((ipcp_ptr->LOPT.ADDR & IN_CLASSC_NET) + 1);      //ipcp_ptr->GATE_PARMS.address = ipcp_ptr->POPT.ADDR;      ipcp_ptr->GATE_PARMS.network = INADDR_ANY;      ipcp_ptr->GATE_PARMS.netmask = INADDR_ANY;      /* Start CR 1133 */      ipcp_ptr->GATE_PARMS.locmask = 0;      /* End CR 1133 */      RTCSCMD_smartissue(ipcp_ptr->GATE_PARMS, IPIF_gate_add);   } /* Endif */#if RTCSCFG_ENABLE_DNS || RTCSCFG_ENABLE_LWDNS   /* Set up the primary DNS server */   if (ipcp_ptr->NEG.NEG_DNS) {#if RTCSCFG_ENABLE_DNS      /* Start CR 2257 */      DNS_SLIST_STRUCT slist_entry;      DNS_init_slist_entry(&slist_entry);      slist_entry.IPADDR = ipcp_ptr->LOPT.DNS;      if (DNS_add_slist_entry(&slist_entry) != DNS_OK)         return FALSE;      /* End CR 2257 */#else      LWDNS_server_ipaddr = ipcp_ptr->LOPT.DNS;#endif   } /* Endif */#endif   if (ipcp_ptr->IP_UP) {      ipcp_ptr->IP_UP(ipcp_ptr->IP_PARAM);   } /* Endif */   return TRUE;} /* Endbody */

 

0 项奖励
回复
1,235 次查看
netra
Contributor IV

Can u please tell me what does this statement  " ipcp_ptr->GATE_PARMS.address = ipcp_ptr->POPT.ADDR?ipcp_ptr->POPT.ADDR:((ipcp_ptr->LOPT.ADDR & IN_CLASSC_NET) + 1);   "     exactly do?

when ppp_up() get executed?

0 项奖励
回复
1,235 次查看
sumate
Contributor I

Great work, Thak you so much.

0 项奖励
回复