PHY Interface for K60

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PHY Interface for K60

2,249 次查看
davidboyd
Contributor I


Hi,

I'm designing hardware that interfaces a K60P100M100 MCU with an Ethernet physical interface.  I am looking for a reference design that includes the connection details of the PHY chip (such as a KSZ8041NL) to the K60, including the optimal configuration for clocks etc....  Probably an RMII rather than MII interface.

The TWR-SER board has lots of superfluous links and configuration options which I'm finding confusing as a reference design.  For example I don't believe I would need the NB2304 clock distribution chip if both the MCU and PHY are running from a single 50MHz clock.

Some references have also indicated that the RMII mode is preferred as there is overlap on some devices with the JTAG interface.

Can anyone point me to a schematic for this already done on the same PCB?  Help appreciated.

David

标签 (1)
0 项奖励
回复
2 回复数

1,850 次查看
mehmetekici
Contributor II

David,

There is only one pin multiplexed between JTAG and RMII_RXER. Pin 39 JTAG_TRST , RMII_RXER. RMII_RXER is optional pin for RMII interface and JTAG_TRST is optional for JTAG. I think you can use whatever funtion you like. There is an errata for some slicon version for RXER too.

I suggest you to check TWR-K60N512 kit reference. I have started a new design similar to one you have. I use K60N512.

Mehmet

0 项奖励
回复

1,850 次查看
Mohsin455
Contributor IV

              Do check that if you are going to use USB, you will need the K60 to be running at 96MHz as the USB requires a clock of 48 MHz.

In the above setup the MII interface would require a separate clock. Not sure about RMII clock requirement, so do check on this.

Mohsin

0 项奖励
回复