PE_demo for KDS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PE_demo for KDS

1,117 Views
philippelequeau
Contributor I

Hi all,

My problem seems to be like this How to set up BSP for PEx in KDS

I'm using KDS2.0.0 and MQX_4_1.

I would like to build the pe_demo exemple to run on a twrk60f120m board.

The problem is that it requires a PEx based BSP and I'm not able to find it.

Where am I false ?

Thank you for the answers

PS: it seems OK when using CodeWarrior 10.6

kds_demo.jpg

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

974 Views
soledad
NXP Employee
NXP Employee

Hello Philippe,

Please check the below thread and let me know if this helps !!!

https://community.freescale.com/docs/DOC-103429


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

974 Views
philippelequeau
Contributor I

Hi Sol,

Thank you.

As I wrote , I'm using TWRK60fK20m board.

The solution you proposed is based on SDK, and there is no SDK available for this board.

I saw that it is recommended to use a superset of the processor and to "adapt" the SDK.

But for this family, there are only two SDKs with a K64F and with a K60D, and none of them is a superset of K60F.

As I don't know how difficult it is ,I'm afraid not have enough time to create this new SDK.

What do you think about that ?

Best  regards

Philippe

0 Kudos
Reply