OS Awareness and MQX Lite

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OS Awareness and MQX Lite

ソリューションへジャンプ
5,255件の閲覧回数
marcbunyard
Contributor IV

What do I need to do to get OS awareness active with MQXLite?  I am using Code Warrior 10.4 Professional Edition with the K20D72M in the TWR-K20D72M, and have the MQXLite component in my project.  I don't know how to get the OS awareness working.  I don't see the OS Awareness Tab under Run->Debug Configurations->Debugger.  During debugging none of the MQX tools is functional.

1 解決策
4,844件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

see attached screenshot of where to enable OS awareness.

元の投稿で解決策を見る

0 件の賞賛
返信
9 返答(返信)
4,845件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

see attached screenshot of where to enable OS awareness.

0 件の賞賛
返信
4,843件の閲覧回数
marcbunyard
Contributor IV

The "OS Awareness" tab doesn't exist on the debugger tab.  I think something is wrong with my installation.  I started with the Special Suite and upgraded to professional.  Could that be blocking the "OS Awareness" tab?

0 件の賞賛
返信
4,843件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

I think that may be the case since I see the option and tried it out successfully on a K60 board. If you don't have a professional license installed properly, then the OS Awareness feature wouldn't available.

Also make sure you have any updates for it installed:


4,843件の閲覧回数
marcbunyard
Contributor IV

Thank you Anthony.  I just tried the site, and it's down.  I'll try later.

0 件の賞賛
返信
4,844件の閲覧回数
Monica
Senior Contributor III

Hello Marc,

just checking up, did you get to try it once the site was up and running? Please keep us posted :smileywink:

Best regards,

Monica

0 件の賞賛
返信
4,844件の閲覧回数
marcbunyard
Contributor IV

I am still unable to get the the site:

http://freescale.com/lgfiles/updates/Eclipse/MCU10_4/com.freescale.mcu.updatesite

I am working with an FAE, and still can't get my installation working correctly.  I'm not sure what the problem is.  Firewall?

0 件の賞賛
返信
4,844件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport


if you can't access this link with online updating. please try to install updates via offline mode. here is the updates download link:

http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_UPDATES_MCU_10_4

here is the update procedure:

http://cache.freescale.com/files/soft_dev_tools/doc/support_info/CW_MCU_SP_QS.pdf

4,844件の閲覧回数
marcbunyard
Contributor IV

Thank you.  I did use the webapp site, and downloaded the updates.  Everything went according to the instructions, but I still don't see the "OS Awareness" tab.  I'm working with someone with the premise that it's a licensing issue.  We'll see.

4,844件の閲覧回数
marcbunyard
Contributor IV

I finally uninstalled Both CodeWarrior and MQX 4.0, then re-installed them starting with CodeWarrior.  Now I have "OS Awareness".  It works for both MQX and MQX Lite.  I don't know what went wrong before, but I was trying to get the MQX 3.8 patch for The AR4100 WiFi board in, and I don't have to do that since it's already in.  So, I don't think I will be touching the environment for a while now.

0 件の賞賛
返信