Number of K24 interrupt priorities?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Number of K24 interrupt priorities?

跳至解决方案
1,741 次查看
fcw
Contributor IV

I'm chasing down what appears to be screwball interrupt responses. Section 3.2.2.1 of the K24 reference manual states the chip has 16 interrupt priority levels. The MQX PSP cortex.h header states  "#define CORTEX_PRIOR_IMPL  (3) " which is manipulated into a left-justified 3-bit mask as required for the NVIC.

- Does the chip have 8 or 16 levels?

- If 16, is the use of 8 by MQX intentional?

标记 (2)
0 项奖励
回复
1 解答
1,626 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi FRED WEDEMEIER

On Cortex-M4 and Cortex-M5 core based platforms, the MQX RTOS interrupt processing is designed this way.

Kinetis K family MCUs support 16 hardware interrupt priority levels. Internally MQX RTOS maps even levels (0,2,4,...,14) for MQX RTOS applications while odd levels (1,3,5,...15) are used internally.

MQX RTOS application interrupt levels are 0 to 7, the mapping from MQX RTOS application levels 0 to 7 to hardware priority levels (0, 2, ..., 14) is implemented in the _bsp_int_init() function.


Have a great day,
Daniel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,627 次查看
fcw
Contributor IV

Got it. Thank you!

0 项奖励
回复
1,627 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi FRED WEDEMEIER

On Cortex-M4 and Cortex-M5 core based platforms, the MQX RTOS interrupt processing is designed this way.

Kinetis K family MCUs support 16 hardware interrupt priority levels. Internally MQX RTOS maps even levels (0,2,4,...,14) for MQX RTOS applications while odd levels (1,3,5,...15) are used internally.

MQX RTOS application interrupt levels are 0 to 7, the mapping from MQX RTOS application levels 0 to 7 to hardware priority levels (0, 2, ..., 14) is implemented in the _bsp_int_init() function.


Have a great day,
Daniel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复