Need analog access guide/manual/hints for TWR-K60D100M ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need analog access guide/manual/hints for TWR-K60D100M ?

Jump to solution
1,229 Views
cronddaemon
Contributor II

Hi,

I have TWR-K60D100M, which has PK60DN512VMD102, MCU.

I want to try with ADC in MQX. I can not able to find more information for Analog section, [ like the PIN nos, init , reading values etc ].

Can anyone tell me , in which PDF/guide , accessing analog is explained ? The document number or link to that document will be very helpful.

Thanks,

Crond


Tags (4)
1 Solution
1,141 Views
c0170
Senior Contributor III

Hello crond deamon,

open MQX reference manual which is located in MQX_installed_folder/doc/mqx (MQX_installed_folder is a path to your MQX installation). There's chapter 8 ADC. Second document is K60 reference manual, link to reference manuals for K60 100MHz:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=K60_100&fpsp=1&tab=Documentation_Tab

Worth to mention, there's ADC example in MQX installation.

Regards,

MartinK

View solution in original post

2 Replies
1,142 Views
c0170
Senior Contributor III

Hello crond deamon,

open MQX reference manual which is located in MQX_installed_folder/doc/mqx (MQX_installed_folder is a path to your MQX installation). There's chapter 8 ADC. Second document is K60 reference manual, link to reference manuals for K60 100MHz:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=K60_100&fpsp=1&tab=Documentation_Tab

Worth to mention, there's ADC example in MQX installation.

Regards,

MartinK

1,141 Views
cronddaemon
Contributor II

thanks. I will use them. :smileyhappy:

0 Kudos
Reply