Need analog access guide/manual/hints for TWR-K60D100M ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Need analog access guide/manual/hints for TWR-K60D100M ?

跳至解决方案
1,226 次查看
cronddaemon
Contributor II

Hi,

I have TWR-K60D100M, which has PK60DN512VMD102, MCU.

I want to try with ADC in MQX. I can not able to find more information for Analog section, [ like the PIN nos, init , reading values etc ].

Can anyone tell me , in which PDF/guide , accessing analog is explained ? The document number or link to that document will be very helpful.

Thanks,

Crond


标记 (4)
1 解答
1,138 次查看
c0170
Senior Contributor III

Hello crond deamon,

open MQX reference manual which is located in MQX_installed_folder/doc/mqx (MQX_installed_folder is a path to your MQX installation). There's chapter 8 ADC. Second document is K60 reference manual, link to reference manuals for K60 100MHz:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=K60_100&fpsp=1&tab=Documentation_Tab

Worth to mention, there's ADC example in MQX installation.

Regards,

MartinK

在原帖中查看解决方案

2 回复数
1,139 次查看
c0170
Senior Contributor III

Hello crond deamon,

open MQX reference manual which is located in MQX_installed_folder/doc/mqx (MQX_installed_folder is a path to your MQX installation). There's chapter 8 ADC. Second document is K60 reference manual, link to reference manuals for K60 100MHz:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=K60_100&fpsp=1&tab=Documentation_Tab

Worth to mention, there's ADC example in MQX installation.

Regards,

MartinK

1,138 次查看
cronddaemon
Contributor II

thanks. I will use them. :smileyhappy:

0 项奖励
回复