Moving interrupt vectors on Kinetis

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Moving interrupt vectors on Kinetis

Jump to solution
2,123 Views
UniversalTroope
Contributor III

I'm having a problem with MQX on the Kinetis K60. I'm trying to generate a periodic interrupt using a Periodic Interface Timer, and that part seems to be working. I can't seem to get the interrupt serviced though.

 

I've compiled MQX with MQX_ROM_VECTORS = 0, and MQX_SPARSE_ISR_TABLE = 0, but according to the NVIC VTOR register, the vectors are still located at 0x00000000. This means I can't install an interrupt outside MQX.

 

How do I get MQX to move the vector table to ram? (I'm using MQX 3.6.2 on IAR EWARM 6.1)

 

Any ideas are welcome!

0 Kudos
Reply
1 Solution
1,511 Views
UniversalTroope
Contributor III

This issue seems to have been resolved in MQX 3.7.

View solution in original post

0 Kudos
Reply
1 Reply
1,512 Views
UniversalTroope
Contributor III

This issue seems to have been resolved in MQX 3.7.

0 Kudos
Reply