MQX products not displaying correctly in SNMP monitoring systems

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MQX products not displaying correctly in SNMP monitoring systems

跳至解决方案
1,466 次查看
jesperevertsson
Contributor IV

Hi, this is a bit of a longshot but we are running out of ideas. In some of our network products we use MQX and the built in SNMP support. Some of our customers have been complaining that those products are not being displayed correctly in their SNMP monotoring systems. They all get listed as ifType 1 (other) which makes the interfaces not dispaly all the data it should. We have done some logging with Wireshark and we can see clearly that 6 (ethernetCsmacd) is sent when we do a configuration poll, but for some reason it's not accepted. For comparrison we did the same thing for some other network products from other manufacturers and they all get displayed correctly. The only real difference we can see between the MQX products and the working products is that they all have two interfaces; one loopback and one ethernet, while MQX only has one. We are not really experts on SNMP so we can't tell if this could be the underlying reason or if we are looking in the wrong place.

The monitoring systems we have tested are NetXMS and Network Node Manager.

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,313 次查看
jesperevertsson
Contributor IV

Hi Daniel, we are using MQX 4.2.0 without any patches. The reason we have not applied the patches is because we've made a lot of fixes ourselves to things that wasn't working correctly in MQX and we don't want them to be overwritten.

With that said we managed to get it to work by adding a loopback interface and then rewriting some snmp response messages that were hard coded to respond only for one interface.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,313 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi Jesper:

Which MQX version you are using? I would suggest you use MQX 4.2.0 with patch 4.2.0.2.

Regards

Daniel

0 项奖励
回复
1,314 次查看
jesperevertsson
Contributor IV

Hi Daniel, we are using MQX 4.2.0 without any patches. The reason we have not applied the patches is because we've made a lot of fixes ourselves to things that wasn't working correctly in MQX and we don't want them to be overwritten.

With that said we managed to get it to work by adding a loopback interface and then rewriting some snmp response messages that were hard coded to respond only for one interface.

0 项奖励
回复