MQX port over MCF5282 eval board need help

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX port over MCF5282 eval board need help

Jump to solution
4,628 Views
francois_boucha
Contributor III

Hello,

 

I'm interested in the MQX OS, especially with the RTCS, but my plateform is the MCF5282 eval. board.

 

So I would like to know if a MQX port for the MCF5282 has been made.

 

If not, what are the steps to do so?

 

Francois 

0 Kudos
Reply
1 Solution
2,895 Views
JuroV
NXP Employee
NXP Employee
_start is routine in CodeWarrior ColdFire's library, whose main purpose is to maintain initialization of memory segments etc.

View solution in original post

0 Kudos
Reply
4 Replies
2,895 Views
EAI
Contributor IV
The MQX/RTCS port for the 5282 is available from Embedded Access. Contact info@embedded-access.com.
0 Kudos
Reply
2,895 Views
francois_boucha
Contributor III

I just need the kernel to run, I don't care about the BSP, I got my own.

 

0 Kudos
Reply
2,895 Views
francois_boucha
Contributor III

In the ___boot sequence, what does _start refers to??  I can't find the file that contains that piece of startup code.  

 

Thanks

 

 

 

0 Kudos
Reply
2,896 Views
JuroV
NXP Employee
NXP Employee
_start is routine in CodeWarrior ColdFire's library, whose main purpose is to maintain initialization of memory segments etc.
0 Kudos
Reply