MQX port over MCF5282 eval board need help

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MQX port over MCF5282 eval board need help

跳至解决方案
4,623 次查看
francois_boucha
Contributor III

Hello,

 

I'm interested in the MQX OS, especially with the RTCS, but my plateform is the MCF5282 eval. board.

 

So I would like to know if a MQX port for the MCF5282 has been made.

 

If not, what are the steps to do so?

 

Francois 

0 项奖励
回复
1 解答
2,890 次查看
JuroV
NXP Employee
NXP Employee
_start is routine in CodeWarrior ColdFire's library, whose main purpose is to maintain initialization of memory segments etc.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,890 次查看
EAI
Contributor IV
The MQX/RTCS port for the 5282 is available from Embedded Access. Contact info@embedded-access.com.
0 项奖励
回复
2,890 次查看
francois_boucha
Contributor III

I just need the kernel to run, I don't care about the BSP, I got my own.

 

0 项奖励
回复
2,890 次查看
francois_boucha
Contributor III

In the ___boot sequence, what does _start refers to??  I can't find the file that contains that piece of startup code.  

 

Thanks

 

 

 

0 项奖励
回复
2,891 次查看
JuroV
NXP Employee
NXP Employee
_start is routine in CodeWarrior ColdFire's library, whose main purpose is to maintain initialization of memory segments etc.
0 项奖励
回复