MQX on k50n512 and with HTTP and SNMP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX on k50n512 and with HTTP and SNMP

802 Views
flaviomituutiar
Contributor I


Hi,

There are some documentation about MQX in k50n512 integrated with HTTP and SNMP?

Thank you.

Best Regards

Flavio

0 Kudos
Reply
1 Reply

664 Views
soledad
NXP Employee
NXP Employee

Hello Flavio,

After install MQX you can find some example application at the next path; you can use these examples as reference,

C:\Freescale\Freescale_MQX_4_2\rtcs\examples

eth_to_serial: Simple character passing between the UART console and the telnet session. Shows custom "lightweight" telnet.

Httpsrv: Simple web server with CGI-like scripts and web pages stored in internal flash.

Shell: Shell command line providing commands for network management.

Snmp: SNMP protocol example providing microprocessor state information.

For HTTP, in the following links you can find more example applications:

http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4417.pdf

http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4345.pdf

http://cache.nxp.com/files/32bit/doc/app_note/AN4022.pdf

Unfortunately we don’t have an example implementing HTTP and SNMP.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply