Hi all,
when I try to generate processor expert code for the Kinetis K60 eval board I get the following error:
"Description Resource Path Location Type
INTERNAL ERROR: Unexpected status of script: Drivers\Common\DeclareISR.prg, please contact Freescale support. bsp_twrk60n512_pe Cpu Processor Expert Errors"
It seems that in CW 10.1 the Processor Expert folder miss this file (and lot of others) that are in CW6.3 but even if i try to copy these files the error still appears.
Can anyone help me on solving this?
Thansk in advance
Solved! Go to Solution.
Hello,
the issue was resolved via email communication with the following result: the issue was originally caused by installing a additional component (e.g. free component from FSL web) that was not compatible with CW V10.x release. In case a similar problem appear, its necessary to delete the follwoing folder on your disk (bak-up it if necessary):
XX:\Users\All Users\Processor Expert\CWMCU_PE5_00
best regards
Vojtech Filip
Processor Expert Support Team
Hello,
could you please post here the project that leads you to getting the error?
best regards
Vojtech Filip
Processor Expert Support Team
Hi Filip,
the project that leads me getting the error is the example project is the example installed with MQX 3.7.
If I build the project without opening the PE folder in the source tree, it build the project successfull, but it I open the PR foulder (e.g to see the elements) or I modify something (add a component) it gives me the error.
Please find it attached.
Kind Regards,
Lorenzo
Hello,
I am sorry, I have not reproduced the internal error reported in Problems window as is described in your original post (in CW V10.1 running under WIN 7 32-bit). My steps were the following:
#1 – Installation of CW V10.x
#2 – Installation of PE update 1.0.1 for CW V10.1 (installation process must end with restart of CW)
#3 – Installation of Compiler patch for MQX V3.7 for CW V10.1 (installation process must end with restart of CW)
#4 – Installation of MQX V3.7 outside of Program files folder (e.g. C:\MQX)
#5 – Importing your project
#6 – Setup of MQX variable for CW – (Linked resource view available through project Properties menu-for details see attached screen-shot)
#7 – Generation of PE code – no issue here
#8 – Building of the whole project – no issue here except two warnings and 2 ignored errors in Problems window (see attached screen-shot)
Could you please try to use the same? Have you used the same steps?
best regards
Vojtech Filip
Processor Expert Support Team
Hello,
The installation procedure is the same I followed,
The only difference is that my MQX install folder is outside Program Files folder but inside a custom folder. (See project:_ref.jpg attached).
If I build the project, without opening bsp_twk60n512_pe it works (see attached build_ok.jpg) but if I Just open the pe tree i Still get the error (see attached build_Nok.jpg).
thanks again in advance,
Lorenzo
Hello,
the only differene I see is in OS and the location of the project. I have checked import of the project directly from the mqx/build/... folder without copying it to my workspace and it worked correctly too. Could you please provide info about your OS and I will try to reproduce the issue there?
Could you plese also try my steps on a fresh 32-bit OS?
best regards
Vojtech Filip
Processor Expert Support Team
Hello,
My os is Windows 7 Home Premium edition x64. I also tried this procedure on a Windows XP Professional x32 and i get the same error.
I wll try to get a windows 7 x32 pc to try the same procedure.
Thanks
Lorenzo
Hello,
the issue was resolved via email communication with the following result: the issue was originally caused by installing a additional component (e.g. free component from FSL web) that was not compatible with CW V10.x release. In case a similar problem appear, its necessary to delete the follwoing folder on your disk (bak-up it if necessary):
XX:\Users\All Users\Processor Expert\CWMCU_PE5_00
best regards
Vojtech Filip
Processor Expert Support Team