MQX lite and bootlaoder

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX lite and bootlaoder

3,175 Views
danielecortella
Contributor V

Hi all,

i have a device with a uTasker Bootlader an MQX lite. I have change the Memory map of the firmware :

MEMORY {

  m_interrupts (RX) : ORIGIN = 0x00008080, LENGTH = 0x00000200

  m_cfmprotrom (RX) : ORIGIN = 0x00008400, LENGTH = 0x00000010

  m_text      (RX) : ORIGIN = 0x00008410, LENGTH = 0x00037BF0

  m_data      (RW) : ORIGIN = 0x1FFFE200, LENGTH = 0x00007E00

}

I know that MQX can copy the interrupt to RAM with the setting MQX_ROM_VECTORS set to 0 in user_config.h. This is necessary for a correct functioning because at 0x00 address i have the bootlaoder. Although this setting the system crash as visible in the image when is execute

#ifdef PEX_RTOS_INIT

    PEX_RTOS_INIT();                   /* Initialization of the selected RTOS. Macro is defined by the RTOS component. */

  #endif

in PE_low_level_init.

Thanks

PS: the system crash in

void _psp_int_install(void)

{

    KERNEL_DATA_STRUCT_PTR kernel_data;

    _GET_KERNEL_DATA(kernel_data);

    __set_MSP((uint_32)kernel_data->INTERRUPT_STACK_PTR);

#if !MQX_ROM_VECTORS

    {

        uint_32         i;

        uint_32_ptr     ptr = (pointer)(&__vect_table);

        /* Initialize the hardware interrupt vector table

         * 0: Initial stack pointer

         * 1: Initial program counter

         */

        for (i = 16; i < PSP_MAXIMUM_INTERRUPT_VECTORS; i++) {

            ptr[i] = (uint_32)_int_kernel_isr;

        }

    }

#endif

}

when the ptr[i] = (uint_32)_int_kernel_isr; is executed

Tags (3)
0 Kudos
Reply
5 Replies

2,788 Views
danielecortella
Contributor V

If i change the setting MQX_ROM_VECTORS  to 1 and add this code in __init_hardware during the initialization

uint32_t *pdst;

  uint32_t *psrc;

  uint16_t i;

  // Then redirect the vector table to RAM by changing the SCB_VTOR like this:

  // Redirect the vector table to the new copy in RAM

  SCB_VTOR = (uint32_t) (0x1FFFE000);

  // Copy Application Stored Interrupt Vector table to RAM

  pdst = (uint32_t*) (0x1FFFE000);

  psrc=(uint32_t*) (0x8080);

  for (i = 0; i < 0xC0; i++, pdst++, psrc++) {

  (*pdst) = (*psrc);

  }

      // Check Copy

      pdst = (uint32_t*) (0x1FFFE000);

      psrc=(uint32_t*) (0x8080);

      for (i = 0; i < 0xC0; i++, pdst++, psrc++) {

          if ((*pdst) != (*psrc)) {

              // error

              while (1) {}

          }

      }

that copy the interrupt table from flash to ram the code is executed but only for a short time, in my function init

void Init_Device(void) {

  int error = 0;

  unsigned int firmware_version_SdCard = 0;

  unsigned int i = 0, bw = 0;

  /*

  * Parte di inizializzazione periferiche del dispositivo

  * ADC, SPI, SDCard

  */

  //Cpu_SetClockConfiguration(0); //setto la cpu alla massima frequenza

  Ref_EN_SetVal();//abilito il MOS sul riferimento del ADC

  //resetto la SdCard agendo sulla alimentazione

  SDCard_ON_ClrVal();

  WAIT_Waitms(10);

  SDCard_ON_SetVal();

when is executed the wait function the cpu crash .... i think is a problem with the systemtimer interrupt of MQX. The crash is visible in the image

Thanks

0 Kudos
Reply

2,788 Views
danielecortella
Contributor V

Hi,

during the __init_hardware i copy the interrupt vector from flash to ram but when the MQX lite is executed with PEX_RTOS_START();  the SCB_VTOR change and return to a wrong value ... Why? Thanks

0 Kudos
Reply

2,788 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Daniele Cortellazi:

I think your copy to RAM is not correct, you should increment both pointers by 4 with each iteration (pdst and psrc).

Apart from that I recommend you to instead give a try to the workaround described in the next post:

How to put vectors in ram with processor expert?

You have the same problem, although I did not try the solution with a bootloader-ready project.

Regards!

Jorge Gonzalez

0 Kudos
Reply

2,788 Views
danielecortella
Contributor V

Setting MQX_ROM_VECTORS to 0 in user_config.h the copy of the interrupt in RAM is not automatic?

Thanks

0 Kudos
Reply

2,788 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hi Daniele:

In the case of MQX Lite, user_config.h is handled by Processor Expert and there is a bug in MQX Lite component that does not allow to install vectors in RAM automatically, you have to apply the workaround of the other thread.

I am sorry for the inconvenience.

Regards!

Jorge Gonzalez

0 Kudos
Reply