MQX flashx 3.8.1 backwards compatibility problem with 3.8.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX flashx 3.8.1 backwards compatibility problem with 3.8.0

776件の閲覧回数
kaskasi
Contributor III

Hello,

Using MQX with K53.

Looks like fopen fails with IO_ERROR after upgrade from the 3.8.0 to 3.8.1. Our project doesn't necessarily need FLASHX so will disable the feature rather than trying to fix it. So please be aware if you have any product out using flashx 3.8.0 and are planning upgrade to 3.8.1.

IO_ERROR happens in flashx.c line 227

return IO_ERROR /* no intersection */

Without spending too much time think it is related to change in flash_ftfl.c function. In 3.8.1 zeroes were added to the block map and maybe that breaks backwards compatibility?!?! Just speculation on my part.

const FLASHX_BLOCK_INFO_STRUCT _flashx_kinetisN_block_map[] = {

    { BSP_INTERNAL_FLASH_SIZE / BSP_INTERNAL_FLASH_SECTOR_SIZE / 2,(_mem_size) BSP_INTERNAL_FLASH_BASE                              , BSP_INTERNAL_FLASH_SECTOR_SIZE, 0 },

    { BSP_INTERNAL_FLASH_SIZE / BSP_INTERNAL_FLASH_SECTOR_SIZE / 2,(_mem_size) BSP_INTERNAL_FLASH_BASE + BSP_INTERNAL_FLASH_SIZE / 2, BSP_INTERNAL_FLASH_SECTOR_SIZE, 0 },

    { 0, 0, 0 }

};

Hope this helps someone,

Kari

タグ(3)
0 件の賞賛
返信
0 返答(返信)