Hello,
I'm attempting to get the polled I2C to work using MQX on the K60 tower. I've gone through the i2c demo and I can see that it appears to be working from the generated output, however I see nothing on the I2C lines.
I'm now attempting to use the tower to talk to another I2C device however it is not working, and after connecting an Oscilloscope to what I believe are the I2C SDA and I2C SCL I'm not seeing any activity.
I'm not sure if I need to change something in the demo to make it output through the tower or if something else may be wrong. I've connected the probes (using Jumpers) to:
SCL: TWRPI I2C SCL (J5 Pin 3)
SDA: TWRPI I2C SDA (J5 Pin 4)
GND: TWRPI J5 Pin 2 GND
Both SCL and SDA pins read at a constant 3.2V.
For MQX I haven't made many or any changes to the actual i2c demo but I have gone into the user config and set:
#define BSPCFG_ENABLE_I2C1 1 (was previously 0)
#define BSPCFG_ENABLE_II2C1 1 (was previously 0)
And then re-compiled the MQX kernel.
Any help moving this along so that I can start actually working with the communications between the two devices instead of just turning them on would be greatly appreciated.
Attached is a txt file log of the i2c demo output.
Thanks,
Nicholas Alunni