MQX Vybrid support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX Vybrid support

2,195 Views
POSterminalPCI_
Contributor II

Dear Sir/Madam,

Hello,

Is MQX available for Vybrid processors?. If not when it will be available?

Is there ISO 7816 support for MQX?

Best regards.

Mehmet Ali Ipin

Labels (1)
Tags (1)
5 Replies

1,097 Views
c0170
Senior Contributor III

Hello Mehmet Ali Ipin,

VYBRID processors are going to be supported in next MQX release which should be released in Q2 2013.

Regards,

MartinK

1,097 Views
POSterminalPCI_
Contributor II

Dear Martin,

Thank you for your answer,

Is it for only Cortex M4 or, Cortex A5-specially VF3XX also supported?

Thanks and best regards.

0 Kudos

1,097 Views
c0170
Senior Contributor III

Hello,

VF6XX will be supported in the MQX.

Regards,

MartinK

0 Kudos

1,097 Views
JohnGoodman
Contributor I

So does that means MQX will support VF5XX that has a Cortex-A5 only?

0 Kudos

1,097 Views
hongtranduc
Contributor II

To be more specific, the MQX is supported Cortex-M4 already, and Cortex-A5 will be supported in this year release.