MQX USB stack with vendor specific class

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX USB stack with vendor specific class

1,410 Views
diegobovi
Contributor I

Hello,

I'm trying to interface a Telit LE920 module to a custom board with a ColdFire CPU and MQX 3.8 via USB.

This module generates 5 serial port on my PC but when I connect it to my board, nothing happens.

Defining _HOST_DEBUG i found that the module is recognized, but the stack doesn't find any match in the driver info table.

So I modify the driver info table as follows:

static  USB_HOST_DRIVER_INFO DriverInfoTable[] =

{

   {

      {0x00,0x00},                  /* Vendor ID per USB-IF             */

      {0x00,0x00},                  /* Product ID per manufacturer      */

      0xFF,//USB_CLASS_COMMUNICATION,      /* Class code                       */

      0xFF,//USB_SUBCLASS_COM_ABSTRACT,    /* Sub-Class code                   */

      0xFF,                         /* Protocol                         */

      0,                            /* Reserved                         */

      usb_host_cdc_acm_event        /* Application call back function   */

...

Now the stack calls the function usb_host_cdc_acm_event() but it is not able to find the class to use because it's value is 0xFF from the device descriptor ( it's 0xFF also on my PC ).

What I have to do to handle the Vendor Specific Class? I fails in the function _usb_hostdev_select_interface().

The source code i'm using is in the folder host\example\cdc\cdc_serial\cdc_serial.c

Thank you

Diego

0 Kudos
Reply
2 Replies

1,179 Views
CarlFST60L
Senior Contributor II

Hi,

How did you go with this project? Has any one else got the serial CDC driver working with Telit modules?

I am looking to start a new project using my MQX design and adding the telit module to the USB port. What is involved in getting the CDC driver working so the serial ports work?

0 Kudos
Reply

1,179 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Diego:

Freescale only supports audio, cdc, hid, msd, phdc classes. not supports vendor specific  class,  you need to implement vendor specific class by yourself.

0 Kudos
Reply