Hello
Documentation and code warrior examples seems typically poor regarding the USB Device Software
I was wondering if anybody has had success in a Composite Class USB Device using the following classes :-
HID - (keyboard)
CDC - (serial comms)
MSD - (mass storage)
If so could anybody please supply code examples
A second question is it possible to have 2 or 3 CDC in the same USB Device. ie USB to 3 serial ports
Thanks in advance
Paul H
Solved! Go to Solution.
Hi Paul,
Here is the answer I received to a service request I opened few weeks ago:
My application should have two virtual serial ports on a single USB device. At this time the enumeration process is ok, the first port works fine, but the second one cannot be opened (for example in Hyperterminal).
Teckna
Hi Paul,
Here is the answer I received to a service request I opened few weeks ago:
My application should have two virtual serial ports on a single USB device. At this time the enumeration process is ok, the first port works fine, but the second one cannot be opened (for example in Hyperterminal).
Teckna
I'm trying to implement composite USB device having CDC plus MST. Does anybody know, if the answer from Spoiler is also vaild for MQX 3.8?