MQX RTOS program always got stuck in "_mqx_idle_task"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX RTOS program always got stuck in "_mqx_idle_task"

ソリューションへジャンプ
7,360件の閲覧回数
titusstalin
Contributor V

HI All,

I'm working with FRDMK64F board.

Not able to debug and run any RTOS code on this board.

Always got stuck at "_mqx_idle_task" function.

It was working perfectly yesterday.

Just today I was soldered the board for for VIN line power up and did some RTC section.

I have two board with the same condition.

I hope it could be some hardware problem.

Please note that I'm able to run the "helloworld_k64f.bin" LED code on that problematic board.

Could any one help me to address this problem.

Any insights on this and it will be greatly appreciated?

Regards,

Titus S.

1 解決策
6,652件の閲覧回数
titusstalin
Contributor V

Hi David,

Thank you so much for your support so far.

Yes, I've checked the pictures and confirmed that I'm using the same board.

Yes, I'm not able to get anything on console (terminal) since it is not able to execute any tasks so its hung at "idletask"

Just now I got new board and its working flawlessly. So no issues with terminal or RTOS code or our won sw code etc.,

My problematic board version is "700-28163 REV A"

New board version is "700-28163 REV C"

I have two problematic boards, I've discussed with hw team and we probed each and every power sections, seems good.

I've no idea on this issue, its mysterious, :-)

I can run every code on my new board.

The problem is started when I've soldered the board for some requirements but its working good for a couple of weeks then stopped working, I given in the following link which I communicated in forums for various requirements and issues.

https://developer.mbed.org/questions/6766/Not-able-to-drive-5V-for-my-RFID-reader-/

https://developer.mbed.org/questions/6465/RTC-connection-for-FRDMK64F/

http://developer.mbed.org/questions/6109/How-to-supply-the-external-power-to-the-/?sort=date

Anything I want to probe/check on hardware side for this issue.

元の投稿で解決策を見る

0 件の賞賛
返信
32 返答(返信)
2,014件の閲覧回数
titusstalin
Contributor V

Hi David,

Thanks for your support so far.

I've tried already with newly created MBED setup and asked m colleague to try and nothing worked out. :-(

One last help :-)

Could you build and generate binary for the following MQX RTOS application.

Actually, I'm using the project based on the RTCS SHELL app on KDS IDE.

C:\Freescale\Freescale_MQX_4_1\rtcs\examples\shell\build\kds\rtcs_shell_frdmk64f

0 件の賞賛
返信
2,014件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Titus,

Attached is C:\Freescale\Freescale_MQX_4_1_1_GA\rtcs\examples\shell for frdm-k64f that has MBED debugger interface.

Baud is 115200.

Here is a short terminal output:

Serial port COM10 opened

Initialized Ram Disk to a:\

NOT A DOS DISK! You must format to continue.

Shell (build: Apr  8 2015)

Copyright (c) 2013 Freescale Semiconductor;

shell>

shell> ipconfig 0 init

Ethernet device 0 initialization successful.

shell>

shell> ipconfig dhcp

Bind via dhcp successful.

shell>

shell> ipconfig

Eth#     : 0

Link     : on

MAC      : 00:00:5e:00:00:00

IP4      : 10.85.1.26 Type: DHCPNOAUTO

IP4 Mask : 255.255.255.0

IP4 Gate : 10.85.1.254

IP4 DNS  : 10.81.250.10

Link status task stopped

shell>

shell>

Regards,

David

0 件の賞賛
返信
2,014件の閲覧回数
titusstalin
Contributor V

Thanks Dave.

Its not working. :-(

0 件の賞賛
返信
2,014件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Titus,

Are you sure you have updated the MBED firmware on the frdm-k64f?

I'm attaching what I have installed recently with fingers and toes crossed.

Out of other ideas.  Might sprinkle Holy water on it or try slamming it on the desk ;-)

I'm also attaching pictures of my FRDM-K64F front and back for you to compare against.

Regards,

David

2,014件の閲覧回数
titusstalin
Contributor V

Might sprinkle Holy water on it or try slamming it on the desk

:-) :-)

I'll try that too ;-)

Thanks for your excellent support Dave.

This is the board I have.

Yes, I've updated the latest firmware, in fact, you shared this in old post already :-)

Okay. I've ordered one more, I'm scared that if new board stuck with this issues then thats it.

May be you can escalate to hw people or ask your colleagues who are worked with this board.

Shall I replace the MCU on board and try ?

Or is it need any firmware inside or just replace the MCU MK64FN

0 件の賞賛
返信
2,014件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Titus,

One last attempt before I scream for help as well.

First I included the firmware again just to be sure you tried it since we've had many posts I thought the other one might have been missed.

Second did the pictures reveal any differences?

Back to the question at hand.  Is the only issue not seeing the terminal output?

If yes, what terminal utility are you using?

Lastly the boards as cheap so I wouldn't recommend trying to replace the MCU since the board might be the issue anyways.

Regards,

David

0 件の賞賛
返信
6,653件の閲覧回数
titusstalin
Contributor V

Hi David,

Thank you so much for your support so far.

Yes, I've checked the pictures and confirmed that I'm using the same board.

Yes, I'm not able to get anything on console (terminal) since it is not able to execute any tasks so its hung at "idletask"

Just now I got new board and its working flawlessly. So no issues with terminal or RTOS code or our won sw code etc.,

My problematic board version is "700-28163 REV A"

New board version is "700-28163 REV C"

I have two problematic boards, I've discussed with hw team and we probed each and every power sections, seems good.

I've no idea on this issue, its mysterious, :-)

I can run every code on my new board.

The problem is started when I've soldered the board for some requirements but its working good for a couple of weeks then stopped working, I given in the following link which I communicated in forums for various requirements and issues.

https://developer.mbed.org/questions/6766/Not-able-to-drive-5V-for-my-RFID-reader-/

https://developer.mbed.org/questions/6465/RTC-connection-for-FRDMK64F/

http://developer.mbed.org/questions/6109/How-to-supply-the-external-power-to-the-/?sort=date

Anything I want to probe/check on hardware side for this issue.

0 件の賞賛
返信
2,014件の閲覧回数
DavidS
NXP Employee
NXP Employee

Very happy new board is operating correctly.

Thank you for letting me know.

Very sorry for the issues you had.

Regards,

David

0 件の賞賛
返信
2,014件の閲覧回数
titusstalin
Contributor V

Thanks Dave.

Could you please escalate this to factory team or DEV team for this problem.

I'm more afraid if my new board get into this issue.

This issue should not happen on my new board after I done hw changes.

So I more concerned on root cause of this problem.

0 件の賞賛
返信
2,014件の閲覧回数
titusstalin
Contributor V

Hi David,

Also I'm attaching the log when I debug the FRDMK64 board through JLINK interface (JLink_OpenSDA_V2 binary used).

Could you check out this and helps to findout the problem(root cause)

Sorry for text paste since I don't know how to attach the file.

SEGGER J-Link GDB Server V4.92 Command Line Version

JLinkARM.dll V4.92 (DLL compiled Sep 30 2014 09:33:42)

-----GDB Server start settings-----

GDBInit file:                  none

GDB Server Listening port:     2331

SWO raw output listening port: 2332

Terminal I/O port:             2333

Accept remote connection:      localhost only

Generate logfile:              off

Verify download:               on

Init regs on start:            on

Silent mode:                   off

Single run mode:               on

Target connection timeout:     5 sec.

------J-Link related settings------

J-Link Host interface:         USB

J-Link script:                 none

J-Link settings file:          none

------Target related settings------

Target device:                 MK64FN1M0xxx12

Target interface:              SWD

Target interface speed:        30kHz

Target endian:                 little

Connecting to J-Link...

J-Link is connected.

Firmware: J-Link OpenSDA 2 compiled Nov 28 2014 10:34:59

Hardware: V1.00

S/N: 621000000

Checking target voltage...

Target voltage: 3.30 V

Listening on TCP/IP port 2331

Connecting to target...Connected to target

Waiting for GDB connection...Connected to 127.0.0.1

Reading all registers

Read 4 bytes @ address 0x00000000 (Data = 0x20030000)

Target interface speed set to 30 kHz

Resetting target

Halting target CPU...

...Target halted (PC = 0x00000560)

R0 = 00000000, R1 = 00000000, R2 = 00000000, R3 = 00000000

R4 = 00000000, R5 = 00000000, R6 = 00000000, R7 = 00000000

R8 = 00000000, R9 = 00000000, R10= 00000000, R11= 00000000

R12= 00000000, R13= 20030000, MSP= 20030000, PSP= 00000000

R14(LR) = FFFFFFFF, R15(PC) = 00000560

XPSR 01000000, APSR 00000000, EPSR 01000000, IPSR 00000000

CFBP 00000000, CONTROL 00, FAULTMASK 00, BASEPRI 00, PRIMASK 00

Reading all registers

Select auto target interface speed (1429 kHz)

Flash breakpoints enabled

Semi-hosting enabled (VectorAddr = 0x08)

Wrong client mask. Semihosting I/O not changed.

SWO disabled succesfully.

Failed to enable SWO. Could not determine a suitable SWO speed!

Downloading 1024 bytes @ address 0x00000000 - Verified OK

Downloading 16 bytes @ address 0x00000400 - Verified OK

Downloading 16160 bytes @ address 0x00000420 - Verified OK

Downloading 16080 bytes @ address 0x00004340 - Verified OK

Downloading 15984 bytes @ address 0x00008210 - Verified OK

Downloading 16240 bytes @ address 0x0000C080 - Verified OK

Downloading 16096 bytes @ address 0x0000FFF0 - Verified OK

Downloading 16128 bytes @ address 0x00013ED0 - Verified OK

Downloading 16128 bytes @ address 0x00017DD0 - Verified OK

Downloading 16208 bytes @ address 0x0001BCD0 - Verified OK

Downloading 16096 bytes @ address 0x0001FC20 - Verified OK

Downloading 16224 bytes @ address 0x00023B00 - Verified OK

Downloading 16160 bytes @ address 0x00027A60 - Verified OK

Downloading 16128 bytes @ address 0x0002B980 - Verified OK

Downloading 16112 bytes @ address 0x0002F880 - Verified OK

Downloading 16160 bytes @ address 0x00033770 - Verified OK

Downloading 16096 bytes @ address 0x00037690 - Verified OK

Downloading 16064 bytes @ address 0x0003B570 - Verified OK

Downloading 16176 bytes @ address 0x0003F430 - Verified OK

Downloading 16080 bytes @ address 0x00043360 - Verified OK

Downloading 15936 bytes @ address 0x00047230 - Verified OK

Downloading 16144 bytes @ address 0x0004B070 - Verified OK

Downloading 16304 bytes @ address 0x0004EF80 - Verified OK

Downloading 16352 bytes @ address 0x00052F30 - Verified OK

Downloading 1868 bytes @ address 0x00056F10 - Verified OK

Downloading 8 bytes @ address 0x0005765C - Verified OK

Downloading 2220 bytes @ address 0x00057664 - Verified OK

Writing register (PC = 0x0000a358)

Read 4 bytes @ address 0x0000A358 (Data = 0x49134812)

Read 2 bytes @ address 0x0003427C (Data = 0xF246)

Read 2 bytes @ address 0x0003427E (Data = 0x305C)

Read 2 bytes @ address 0x00034280 (Data = 0xF2C0)

Read 2 bytes @ address 0x00034282 (Data = 0x0005)

Read 2 bytes @ address 0x0003427C (Data = 0xF246)

Read 2 bytes @ address 0x0003427C (Data = 0xF246)

Read 2 bytes @ address 0x0003427E (Data = 0x305C)

Read 2 bytes @ address 0x00034280 (Data = 0xF2C0)

Read 2 bytes @ address 0x00034282 (Data = 0x0005)

Read 2 bytes @ address 0x0003427C (Data = 0xF246)

Read 2 bytes @ address 0x0003427E (Data = 0x305C)

Read 2 bytes @ address 0x00034280 (Data = 0xF2C0)

Read 2 bytes @ address 0x00034282 (Data = 0x0005)

Read 2 bytes @ address 0x0003427C (Data = 0xF246)

Resetting target

Halting target CPU...

...Target halted (PC = 0x0000A358)

R0 = 00000000, R1 = 00000000, R2 = 00000000, R3 = 00000000

R4 = 00000000, R5 = 00000000, R6 = 00000000, R7 = 00000000

R8 = 00000000, R9 = 00000000, R10= 00000000, R11= 00000000

R12= 00000000, R13= 2002FC00, MSP= 2002FC00, PSP= 00000000

R14(LR) = FFFFFFFF, R15(PC) = 0000A358

XPSR 01000000, APSR 00000000, EPSR 01000000, IPSR 00000000

CFBP 00000000, CONTROL 00, FAULTMASK 00, BASEPRI 00, PRIMASK 00

Reading all registers

Read 4 bytes @ address 0x0000A358 (Data = 0x49134812)

Setting breakpoint @ address 0x0003427C, Size = 2, BPHandle = 0x0002

Starting target CPU...

...Breakpoint reached @ address 0x0003427C

Reading all registers

Removing breakpoint @ address 0x0003427C, Size = 2

Read 4 bytes @ address 0x0003427C (Data = 0x305CF246)

Reading 64 bytes @ address 0x2002FBC0

0 件の賞賛
返信
2,014件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Titus,

Here is my output...their are differences...

SEGGER J-Link GDB Server V4.92 Command Line Version

JLinkARM.dll V4.92 (DLL compiled Sep 30 2014 09:33:42)

-----GDB Server start settings-----

GDBInit file:                  none

GDB Server Listening port:     2331

SWO raw output listening port: 2332

Terminal I/O port:             2333

Accept remote connection:      localhost only

Generate logfile:              off

Verify download:               on

Init regs on start:            on

Silent mode:                   off

Single run mode:               on

Target connection timeout:     5 sec.

------J-Link related settings------

J-Link Host interface:         USB

J-Link script:                 none

J-Link settings file:          none

------Target related settings------

Target device:                 MK64FN1M0xxx12

Target interface:              SWD

Target interface speed:        30kHz

Target endian:                 little

Connecting to J-Link...

J-Link is connected.

Firmware: J-Link OpenSDA 2 compiled Apr 24 2014 14:44:11

Hardware: V1.00

S/N: 621000000

Checking target voltage...

Target voltage: 3.30 V

Listening on TCP/IP port 2331

Connecting to target...Connected to target

Waiting for GDB connection...Connected to 127.0.0.1

Reading all registers

Read 4 bytes @ address 0x00000000 (Data = 0x20030000)

Target interface speed set to 30 kHz

Resetting target

Halting target CPU...

...Target halted (PC = 0x00000410)

R0 = 00000000, R1 = 00000000, R2 = 00000000, R3 = 00000000

R4 = 00000000, R5 = 00000000, R6 = 00000000, R7 = 00000000

R8 = 00000000, R9 = 00000000, R10= 00000000, R11= 00000000

R12= 00000000, R13= 20030000, MSP= 20030000, PSP= 00000000

R14(LR) = FFFFFFFF, R15(PC) = 00000410

XPSR 01000000, APSR 00000000, EPSR 01000000, IPSR 00000000

CFBP 00000000, CONTROL 00, FAULTMASK 00, BASEPRI 00, PRIMASK 00

Reading all registers

Select auto target interface speed (1429 kHz)

Flash breakpoints enabled

Downloading 1024 bytes @ address 0x00000000 - Verified OK

Downloading 16 bytes @ address 0x00000400 - Verified OK

Downloading 16096 bytes @ address 0x00000410 - Verified OK

Downloading 16144 bytes @ address 0x000042F0 - Verified OK

Downloading 5368 bytes @ address 0x00008200 - Verified OK

Downloading 8 bytes @ address 0x000096F8 - Verified OK

Downloading 2172 bytes @ address 0x00009700 - Verified OK

Read 4 bytes @ address 0x00000410 (Data = 0x49124811)

Read 2 bytes @ address 0x000006EC (Data = 0xF005)

Read 2 bytes @ address 0x000006EC (Data = 0xF005)

Read 2 bytes @ address 0x00000000 (Data = 0x0000)

Read 2 bytes @ address 0x00000002 (Data = 0x2003)

Read 2 bytes @ address 0x00000004 (Data = 0x0411)

Read 2 bytes @ address 0x00000006 (Data = 0x0000)

Read 2 bytes @ address 0x00000008 (Data = 0x0685)

Read 2 bytes @ address 0x0000000A (Data = 0x0000)

Read 2 bytes @ address 0x0000000C (Data = 0x0685)

Read 2 bytes @ address 0x0000000E (Data = 0x0000)

Read 2 bytes @ address 0x00000010 (Data = 0x0685)

Read 2 bytes @ address 0x00000012 (Data = 0x0000)

Read 2 bytes @ address 0x00000014 (Data = 0x0685)

Read 2 bytes @ address 0x00000016 (Data = 0x0000)

Read 2 bytes @ address 0x00000018 (Data = 0x0685)

Read 2 bytes @ address 0x0000001A (Data = 0x0000)

Read 2 bytes @ address 0x0000001C (Data = 0x0000)

Read 2 bytes @ address 0x0000001E (Data = 0x0000)

Read 2 bytes @ address 0x00000020 (Data = 0x0000)

Read 2 bytes @ address 0x00000022 (Data = 0x0000)

Read 2 bytes @ address 0x00000024 (Data = 0x0000)

Read 2 bytes @ address 0x00000026 (Data = 0x0000)

Read 2 bytes @ address 0x00000028 (Data = 0x0000)

Read 2 bytes @ address 0x0000002A (Data = 0x0000)

Read 2 bytes @ address 0x0000002C (Data = 0x0499)

Read 2 bytes @ address 0x0000002E (Data = 0x0000)

Read 2 bytes @ address 0x00000030 (Data = 0x0685)

Read 2 bytes @ address 0x00000032 (Data = 0x0000)

Read 2 bytes @ address 0x00000034 (Data = 0x0000)

Read 2 bytes @ address 0x00000036 (Data = 0x0000)

Read 2 bytes @ address 0x00000038 (Data = 0x051B)

Read 2 bytes @ address 0x0000003A (Data = 0x0000)

Read 2 bytes @ address 0x0000003C (Data = 0x0455)

Read 2 bytes @ address 0x0000003E (Data = 0x0000)

Read 2 bytes @ address 0x00000040 (Data = 0x0685)

Read 2 bytes @ address 0x00000042 (Data = 0x0000)

Read 2 bytes @ address 0x00000044 (Data = 0x0685)

Read 2 bytes @ address 0x00000046 (Data = 0x0000)

Read 2 bytes @ address 0x00000048 (Data = 0x0685)

Read 2 bytes @ address 0x0000004A (Data = 0x0000)

Read 2 bytes @ address 0x0000004C (Data = 0x0685)

Read 2 bytes @ address 0x0000004E (Data = 0x0000)

Resetting target

Halting target CPU...

...Target halted (PC = 0x00000410)

Read 2 bytes @ address 0x000006EC (Data = 0xF005)

Read 2 bytes @ address 0x000006EC (Data = 0xF005)

Read 2 bytes @ address 0x000006EC (Data = 0xF005)

R0 = 00000000, R1 = 00000000, R2 = 00000000, R3 = 00000000

R4 = 00000000, R5 = 00000000, R6 = 00000000, R7 = 00000000

R8 = 00000000, R9 = 00000000, R10= 00000000, R11= 00000000

R12= 00000000, R13= 20030000, MSP= 20030000, PSP= 00000000

R14(LR) = FFFFFFFF, R15(PC) = 00000410

XPSR 01000000, APSR 00000000, EPSR 01000000, IPSR 00000000

CFBP 00000000, CONTROL 00, FAULTMASK 00, BASEPRI 00, PRIMASK 00

Reading all registers

Read 4 bytes @ address 0x00000410 (Data = 0x49124811)

Setting breakpoint @ address 0x000006EC, Size = 2, BPHandle = 0x0001

Starting target CPU...

...Breakpoint reached @ address 0x000006EC

Reading all registers

Removing breakpoint @ address 0x000006EC, Size = 2

Read 4 bytes @ address 0x000006EC (Data = 0xFBE2F005)

Reading 64 bytes @ address 0x2002FFC0

Read 2 bytes @ address 0x00000000 (Data = 0x0000)

Read 2 bytes @ address 0x00000002 (Data = 0x2003)

Read 2 bytes @ address 0x00000004 (Data = 0x0411)

Read 2 bytes @ address 0x00000006 (Data = 0x0000)

Read 2 bytes @ address 0x00000008 (Data = 0x0685)

Read 2 bytes @ address 0x0000000A (Data = 0x0000)

Read 2 bytes @ address 0x0000000C (Data = 0x0685)

Read 2 bytes @ address 0x0000000E (Data = 0x0000)

Read 2 bytes @ address 0x00000010 (Data = 0x0685)

Read 2 bytes @ address 0x00000012 (Data = 0x0000)

Read 2 bytes @ address 0x00000014 (Data = 0x0685)

Read 2 bytes @ address 0x00000016 (Data = 0x0000)

Read 2 bytes @ address 0x00000018 (Data = 0x0685)

Read 2 bytes @ address 0x0000001A (Data = 0x0000)

Read 2 bytes @ address 0x0000001C (Data = 0x0000)

Read 2 bytes @ address 0x0000001E (Data = 0x0000)

Read 2 bytes @ address 0x00000020 (Data = 0x0000)

Read 2 bytes @ address 0x00000022 (Data = 0x0000)

Read 2 bytes @ address 0x00000024 (Data = 0x0000)

Read 2 bytes @ address 0x00000026 (Data = 0x0000)

Read 2 bytes @ address 0x00000028 (Data = 0x0000)

Read 2 bytes @ address 0x0000002A (Data = 0x0000)

Read 2 bytes @ address 0x0000002C (Data = 0x0499)

Read 2 bytes @ address 0x0000002E (Data = 0x0000)

Read 2 bytes @ address 0x00000030 (Data = 0x0685)

Read 2 bytes @ address 0x00000032 (Data = 0x0000)

Read 2 bytes @ address 0x00000034 (Data = 0x0000)

Read 2 bytes @ address 0x00000036 (Data = 0x0000)

Read 2 bytes @ address 0x00000038 (Data = 0x051B)

Read 2 bytes @ address 0x0000003A (Data = 0x0000)

Read 2 bytes @ address 0x0000003C (Data = 0x0455)

Read 2 bytes @ address 0x0000003E (Data = 0x0000)

Read 2 bytes @ address 0x00000040 (Data = 0x0685)

Read 2 bytes @ address 0x00000042 (Data = 0x0000)

Read 2 bytes @ address 0x00000044 (Data = 0x0685)

Read 2 bytes @ address 0x00000046 (Data = 0x0000)

Read 2 bytes @ address 0x00000048 (Data = 0x0685)

Read 2 bytes @ address 0x0000004A (Data = 0x0000)

Read 2 bytes @ address 0x0000004C (Data = 0x0685)

Read 2 bytes @ address 0x0000004E (Data = 0x0000)

Read 2 bytes @ address 0x000006EC (Data = 0xF005)

Read 2 bytes @ address 0x000006EE (Data = 0xFBE2)

Read 2 bytes @ address 0x000006F0 (Data = 0xF003)

Read 2 bytes @ address 0x000006F2 (Data = 0xFE06)

Read 2 bytes @ address 0x000006F4 (Data = 0xE7FE)

Read 2 bytes @ address 0x000006F4 (Data = 0xE7FE)

Read 2 bytes @ address 0x000006F4 (Data = 0xE7FE)

Read 2 bytes @ address 0x000006F6 (Data = 0xBF00)

Read 2 bytes @ address 0x000006F8 (Data = 0xB580)

Read 2 bytes @ address 0x000006FA (Data = 0xB084)

Read 2 bytes @ address 0x000006FC (Data = 0xAF00)

Read 2 bytes @ address 0x000006FE (Data = 0x6078)

Read 2 bytes @ address 0x00000700 (Data = 0x2301)

Read 2 bytes @ address 0x00000702 (Data = 0x73FB)

Read 2 bytes @ address 0x00000704 (Data = 0x7BFB)

Read 2 bytes @ address 0x00000706 (Data = 0xF648)

Read 2 bytes @ address 0x00000708 (Data = 0x00F4)

Read 2 bytes @ address 0x0000070A (Data = 0xF2C0)

Read 2 bytes @ address 0x0000070C (Data = 0x0000)

Read 2 bytes @ address 0x0000070E (Data = 0x4619)

Read 2 bytes @ address 0x00000710 (Data = 0xF002)

Read 2 bytes @ address 0x00000712 (Data = 0xF844)

Read 2 bytes @ address 0x00000714 (Data = 0xF44F)

Read 2 bytes @ address 0x00000716 (Data = 0x70FA)

Read 2 bytes @ address 0x00000718 (Data = 0xF003)

Read 2 bytes @ address 0x0000071A (Data = 0xFDC4)

Read 2 bytes @ address 0x0000071C (Data = 0xF107)

Read 2 bytes @ address 0x0000071E (Data = 0x030F)

Read 2 bytes @ address 0x00000720 (Data = 0x2004)

Read 2 bytes @ address 0x00000722 (Data = 0x4619)

Read 2 bytes @ address 0x00000724 (Data = 0x2201)

Read 2 bytes @ address 0x00000726 (Data = 0x2300)

Read 2 bytes @ address 0x00000728 (Data = 0xF004)

Read 2 bytes @ address 0x0000072A (Data = 0xFEF4)

Read 2 bytes @ address 0x0000072C (Data = 0x7BFB)

Read 2 bytes @ address 0x0000072E (Data = 0x3301)

Read 2 bytes @ address 0x00000730 (Data = 0xB2DB)

Read 2 bytes @ address 0x00000732 (Data = 0x73FB)

Read 2 bytes @ address 0x00000734 (Data = 0x7BFB)

Read 2 bytes @ address 0x00000736 (Data = 0x2B01)

Read 2 bytes @ address 0x00000738 (Data = 0xD901)

Read 2 bytes @ address 0x0000073A (Data = 0x2300)

Read 2 bytes @ address 0x0000073C (Data = 0x73FB)

Read 2 bytes @ address 0x0000073E (Data = 0xF44F)

Read 2 bytes @ address 0x00000740 (Data = 0x70FA)

Read 2 bytes @ address 0x00000742 (Data = 0xF003)

Read 2 bytes @ address 0x00000744 (Data = 0xFDAF)

Read 2 bytes @ address 0x00000746 (Data = 0xE7DD)

Read 2 bytes @ address 0x00000748 (Data = 0xB480)

Read 2 bytes @ address 0x0000074A (Data = 0xAF00)

Regards,

David

0 件の賞賛
返信
2,014件の閲覧回数
titusstalin
Contributor V

I have followed the same procedure and able to download the binary automatically but that generated binary is not working.

What is going on ? :-)

MBED_example.png

0 件の賞賛
返信