MQX/MQX Lite Context Switching Cycles

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX/MQX Lite Context Switching Cycles

Jump to solution
631 Views
MatthewScott_DE
Contributor II

Does anyone know the amount of cycles it takes to perform a context switch in MQX?  Is MQX Lite any different?

0 Kudos
1 Solution
289 Views
c0170
Senior Contributor III

Hello,

this thread gives you a hint which example to check and david shared also there some numbers:

Re: Minimum Interrupt Latency

Quoted from MQX Real-time Operating System

Depending on platform and options chosen, MQX RTOS can be configured to take as little as 6K bytes of ROM, including kernel, interrupts, semaphores, queues and memory manager. MQX RTOS delivers the performance that demanding customer have come to expect in leading RTOS solutions as well, on a 200 MHz PowerPC® MPC8248, interrupt latency came in at 0.331 µsec and context switch time was benchmarked at 0.558 µsec.

Regards,

c0170

View solution in original post

0 Kudos
1 Reply
290 Views
c0170
Senior Contributor III

Hello,

this thread gives you a hint which example to check and david shared also there some numbers:

Re: Minimum Interrupt Latency

Quoted from MQX Real-time Operating System

Depending on platform and options chosen, MQX RTOS can be configured to take as little as 6K bytes of ROM, including kernel, interrupts, semaphores, queues and memory manager. MQX RTOS delivers the performance that demanding customer have come to expect in leading RTOS solutions as well, on a 200 MHz PowerPC® MPC8248, interrupt latency came in at 0.331 µsec and context switch time was benchmarked at 0.558 µsec.

Regards,

c0170

0 Kudos