MQX_KSDK missing 80-Pin Cases

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MQX_KSDK missing 80-Pin Cases

1,058 次查看
m3
Contributor II

What happened to the 80-Pins QFP types in MQX_KSDK?.Even for the supported MCUs the QFP-80 case is missing.:smileyshocked:

标记 (2)
0 项奖励
回复
2 回复数

986 次查看
soledad
NXP Employee
NXP Employee

Hi m3,

Sorry if I am not understanding your question very well. MQX only has support for Freescale boards, so if the boards do not have 80 pins devices then MQX does not have support for 80 pins devices.

If you have a custom board then you need to create your own BSP. The BSP has the pin definitions.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

986 次查看
m3
Contributor II

Great! Why not putting this info in front of the Webpage? Here is what i believed to be true:

Supported Devices

  • Kinetis K2x USB Microcontrollers (MCUs)
    • K22_100: Kinetis K22 - 100 MHz, Low Power, USB Microcontrollers (MCUs)
    • K22_120: Kinetis K22 - 120 MHz, Low Power, High Performance, USB Microcontrollers (MCUs)
    • K24_120: Kinetis K24 - 120 MHz, Low Power, High Performance, USB, with 256KB SRAM Microcontrollers (MCUs)
  • Kinetis K6x Ethernet Crypto Microcontrollers (MCUs)
    • K63_120: Kinetis K63 - 120 MHz, Ethernet, USB, Security, Tamper Detection, with 256KB SRAM Microcontrollers (MCUs)
    • K64_120: Kinetis K64 - 120 MHz, Ethernet, USB, 256KB SRAM Microcontrollers (MCUs)
  • KV3x: Kinetis KV3x - 100/120 MHz, BLCD, DSP, FPU, High Performance Microcontrollers (MCUs)

Nothing about toy-like boards and since this is freescale.com not lego i have erroneously assumed that we talk about real world applications.

0 项奖励
回复