[MQX]: K20 low power mode with UART on?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[MQX]: K20 low power mode with UART on?

1,225 Views
huishao2
Contributor IV

Hi-

I need to find MQX application notes for power saving on a K20D50M based board. The board needs to stay in low power mode while leaving UART on. Wondering if there is such application notes to help? The system is MQX3.8 powered.

Thanks!

Hui

0 Kudos
Reply
2 Replies

1,068 Views
huishao2
Contributor IV

Hi Sol

Thanks for your reply!

Wondering if there is a more specific app notes with demo code to assist on my application. A k20d50m custom board running MQX4.1. I am trying to make it into low power either with UART active or wake it up by RxD transition.

Regards

Hui

0 Kudos
Reply

1,066 Views
soledad
NXP Employee
NXP Employee

Hello Hui,

Please check the below application note and the doc attached.

Let me know if this helps.

http://cache.nxp.com/files/32bit/doc/app_note/AN4447.pdf


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply