MQX 4.1: USB CDC device "virtual com" not enumerating

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MQX 4.1: USB CDC device "virtual com" not enumerating

跳至解决方案
1,631 次查看
huishao2
Contributor IV

Hi-

I have problem to make my board enumerated after plugging USB connector into Windows PC. Windows shows nothing after a connection. My configuration is like:

OS: MQX 4.1.1

HW: MX20DX128VFM5

Tool: IAR and I-jet

BSP: k20d50m

My costumed board is driven by 8MHz crystal and +5v comes directly from PC USB port. The USB ID detection pin is tied to ground and +5V power is seen on the board after connecting to PC. After calculation my board should supply 48MHz to ARM core.

Code wise, I can see the device  stack is initialized OK.  However, in code below, I don't see start_app and start_transactions are TRUE.

       /* call the periodic task function */
       USB_CDC_Periodic_Task(); 
      
       /*check whether enumeration is complete or not */
       if((start_app==TRUE) && (start_transactions==TRUE))

No sure where to start the investigation, look at the clock init code in bsp_cm.c:

LDD_TError Cpu_SetClockConfiguration(LDD_TClockConfiguration ModeID)

{

  if (ModeID > 0x02U) {

    return ERR_RANGE;                  /* Undefined clock configuration requested requested */

  }

  switch (ModeID) {

case CPU_CLOCK_CONFIG_0:

...

case CPU_CLOCK_CONFIG_1:

...

case CPU_CLOCK_CONFIG_2:

...

}

...

}

Stepping through the clock init code, I see twice of settings are either config_0 and then config_1 (BSP_CLOCK_CONFIGURATION_AUTOTRPM and BSP_CLOCK_CONFIGURATION_DEFAULT?). From there, USB clock prescalers are USBDIV=1 and USBFRAC=0. Is it correct for USB FS?

My operation steps are:

1. connect my board to Windows PC USB port

2. Load code through IAR I-jet

Windows simply doesn't show anything after  the step above? Where should I start to look into this issue?

0 项奖励
回复
1 解答
1,330 次查看
huishao2
Contributor IV

After some investigation work, it seems to be a memory allocation failure inside CDC device initialization due to tight 16KB RAM. But the enumeration issue is still there. Will ask in a different thread.

Thanks!

Hui

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,330 次查看
soledad
NXP Employee
NXP Employee

Hi Hui Shao,

http://cache.freescale.com/files/32bit/hardware_tools/schematics/TWRK20D50M_SCH.pdf?fr=gtl

This is  the link for the twrk20d50 schematic file, could you please check the page 6? In this page you can find the hardware for the USB, could you please doble check it?

This is in order to isolate the issue, I am looking a hardward issue.

In addition, could you please try using the Virtual COM CDC example from MQX, you can find it at the next path:

C:\Freescale\Freescale_MQX_4_1\usb\device\examples\cdc\virtual_com

Have a great day,

Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,331 次查看
huishao2
Contributor IV

After some investigation work, it seems to be a memory allocation failure inside CDC device initialization due to tight 16KB RAM. But the enumeration issue is still there. Will ask in a different thread.

Thanks!

Hui

0 项奖励
回复