Hello,
Can I use MQX 4.1.2 (taken from FSLMQXOS_4_1_2_Vybrid folder, so I presume it’s 4.1.2) on TWR-VF65GS10 rev H? (sticker on the bottom says: SCH-27442 REV H)
I have built the bsp, pep and mcc and linked it to my app. When I load it using mqxboot it hangs half-way through the load
thanks
Solved! Go to Solution.
Hello Tomasz,
Yes, the Vybrid package was tested with the following hardware configurations:
• X-SVF522R-EVB Vybrid Evaluation Board Rev. B with the SVF522R3MK4 processor.
• TWR-VF65GS10 Development Kit Rev. H with the MVF61NS10MK50 processor.
Could please add a screenshot of this issue?
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Tomasz,
Yes, the Vybrid package was tested with the following hardware configurations:
• X-SVF522R-EVB Vybrid Evaluation Board Rev. B with the SVF522R3MK4 processor.
• TWR-VF65GS10 Development Kit Rev. H with the MVF61NS10MK50 processor.
Could please add a screenshot of this issue?
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
All works fine now with 4.2.0 MQX. thanks