MQX_4_1_2 on TWR-VF65GS10 rev H?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX_4_1_2 on TWR-VF65GS10 rev H?

Jump to solution
1,094 Views
tomaszsliwinski
Contributor III

Hello,

Can I use MQX 4.1.2 (taken from FSLMQXOS_4_1_2_Vybrid folder, so I presume it’s 4.1.2) on TWR-VF65GS10 rev H? (sticker on the bottom says: SCH-27442 REV H)

I have built the bsp, pep and mcc and linked it to my app.  When I load it using mqxboot it hangs half-way through the load

thanks

Tags (3)
0 Kudos
Reply
1 Solution
620 Views
soledad
NXP Employee
NXP Employee

Hello Tomasz,

Yes, the Vybrid package was tested with the following hardware configurations:

• X-SVF522R-EVB Vybrid Evaluation Board Rev. B with the SVF522R3MK4 processor.

• TWR-VF65GS10 Development Kit Rev. H with the MVF61NS10MK50 processor.

Could please add a screenshot of this issue?


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
621 Views
soledad
NXP Employee
NXP Employee

Hello Tomasz,

Yes, the Vybrid package was tested with the following hardware configurations:

• X-SVF522R-EVB Vybrid Evaluation Board Rev. B with the SVF522R3MK4 processor.

• TWR-VF65GS10 Development Kit Rev. H with the MVF61NS10MK50 processor.

Could please add a screenshot of this issue?


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

620 Views
tomaszsliwinski
Contributor III

All works fine now with 4.2.0 MQX.  thanks

0 Kudos
Reply