MQX 3.8 Install problems w CW10.1 for 51JF

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MQX 3.8 Install problems w CW10.1 for 51JF

跳至解决方案
1,074 次查看
Zpilot
Contributor I

Ran the MQX installer which warned that not all debug libraries are loaded.  I followed instructions to load and recompile the MQX 3.8 core libraries.  First problem:

 

When trying to load the _bsp files, the error message "Some projects were hidden because they exist in the workspace directory".  Received the same error for the _usb_device files. All of the others loaded.

 

I then followed the ordering proscribed for recompiling and now the bsp_twrmcf51jf : Debug and cdc_vcom_twrmcf51jf : Int Flash Debug files have the error flag on them and all of the rest of the files have the yellow "warning" icon attached.

 

How to proceed?

 Zpilot

0 项奖励
回复
1 解答
948 次查看
petr_uhlir
NXP Employee
NXP Employee

MCF51JF is not supported in CW 10.1 by default.  Check if you have installed the Service Pack for MCF51Jx/Qx derivatives

from  http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_UPDATES_MCU_10_1

or download and install CW 10.2

 

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
949 次查看
petr_uhlir
NXP Employee
NXP Employee

MCF51JF is not supported in CW 10.1 by default.  Check if you have installed the Service Pack for MCF51Jx/Qx derivatives

from  http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_UPDATES_MCU_10_1

or download and install CW 10.2

 

 

0 项奖励
回复
948 次查看
c0170
Senior Contributor III

Hi Zpilot,

 

which instructions did you follow? What warning/error messages did you receive?

 

You can drag the project to the codewarrior . Go to the mqx\build\cw10\bsp_twrmcf51jf in your case, drag the .project file to the bar Codewarrior Projects.

 

Regards,

MartinK

0 项奖励
回复