MQX 3.8(.1?) using with PE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX 3.8(.1?) using with PE

Jump to solution
1,574 Views
GerasinIvan
Contributor II

Hi all!

I have some problems with using MQX. To introducing into MQX, i used pe_demo. But after "build" i met an error:

#error Demo requires Processor Expert BSP code to be generated.

#error See "<MQX_INSTALL_DIR>\doc\tools\cw\FSL_MQX_in_CW_10_x.pdf" chapter "CW10.x, MQX and Processor Expert" for details

in community i found

Re: Porting Kinetis BSP_pe from MQX 3.7 to MQX 3.8.1

But isn't really helps. So, i need step-by-step instructions to make and launch MQX on kintis. And how i can use PE in this project)

Thx for helping)

0 Kudos
Reply
1 Solution
1,395 Views
Martin_
NXP Employee
NXP Employee

Hi Ivan,

"<MQX_INSTALL_DIR>\doc\tools\cw\FSL_MQX_in_CW_10_x.pdf" chapter "CW10.x, MQX and Processor Expert"

on page 46 there is step 4 "Generate code"

First command PE to Generate code, then build.

View solution in original post

0 Kudos
Reply
2 Replies
1,396 Views
Martin_
NXP Employee
NXP Employee

Hi Ivan,

"<MQX_INSTALL_DIR>\doc\tools\cw\FSL_MQX_in_CW_10_x.pdf" chapter "CW10.x, MQX and Processor Expert"

on page 46 there is step 4 "Generate code"

First command PE to Generate code, then build.

0 Kudos
Reply
1,395 Views
GerasinIvan
Contributor II

Thank you, Martin! It really helps. Now I can work with MQX, i hope) I will fully test it later, but i think it's all right. Thank you, again.

0 Kudos
Reply