I'm using MQX 3.5 on a board based on MCF52259 uC and I use CW7.1.2 to develop final application.
I use the uC USB peripheral in order to connect USB sticks to the board, and I have some problem in USB detection.
In fact, I tried 10 different USB sticks (various types and sizes) and only 5 of them were recognized by the OS. Some of them were not detected at all (no messages on standard output), instead with some others I saw "Unable to open USB disk" message on standard output. All the USB sticks I tried work well on PCs.
I'm thinking about trying to migrate to MQX 3.8. Does anybody know if this is a known issue on MQX 3.5 and if there is some solution?
Thanks in advance
Best regards
解決済! 解決策の投稿を見る。
we finally solved our problem migrating to MQX 3.8 and CW7.2.2.
we figured out the problem was due to a some kind of conflict between our 1ms PIT, in which we put MQX scheduler as suggested in PIT usage example, and USB Task.
i'm having a similar issue using mqx 3.6.1 and mem_extend. we cannot migrate to 3.8 and have to use external ram due to the size and complexity of our application.
we finally solved our problem migrating to MQX 3.8 and CW7.2.2.
we figured out the problem was due to a some kind of conflict between our 1ms PIT, in which we put MQX scheduler as suggested in PIT usage example, and USB Task.
Glad you found a solution.
Are you using external RAM and a common memory pool that spans internal and external RAM. Or are you in internal RAM only?