MK60DN512 vs MK60DN512Z MQX issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK60DN512 vs MK60DN512Z MQX issue

Jump to solution
691 Views
aroste
Contributor IV

Hi,

(CW10.5, MQX4.0.2)

I cloned the BSP TWR-K60N512 for my project that use a MK60DN512VLQ10.

In the BSP tower project it is a MK60DN512Z (define PSP_CPU_MK60DN512Z). I tried to change in PE the processor type (add new and disable the Z) and I have some issues in MQX files. (I2S mainly)

Can someone help me to understand why a uC that should not be used for new design (the Z) is supported in MQX and not the current one?  

Or maybe I am missing something but at this point I loose my minds.  (I checked the reference manual and I can see the difference in the IO_Map.h correspond to the differences in the manual)

I will try now the clone a BSP from the twr-k60d100m now to see the difference.

Thanks

BR

stéphan

Tags (2)
0 Kudos
Reply
1 Solution
407 Views
aroste
Contributor IV

At this point I succeeded by starting from the TWR-K60D100M that is the correct family.  I can see that the BSP files and all io files are related to the non-"Z" version now.    :-)

View solution in original post

0 Kudos
Reply
1 Reply
408 Views
aroste
Contributor IV

At this point I succeeded by starting from the TWR-K60D100M that is the correct family.  I can see that the BSP files and all io files are related to the non-"Z" version now.    :-)

0 Kudos
Reply