I have found a bug in MFS_Open_file the mfs_open.c file. A snippet of the code is shown below:
/* Lookup entry with the requested name in the directory */
error_code = MFS_scan_dir_chain(drive_ptr, &dir_chain, entry_name, &dir_entry, &entry_sector, &entry_index, NULL);
if (error_code == MFS_NO_ERROR)
{
/* Check if it is a regular file and verify permissions */
if (dir_entry.ATTRIBUTE[0] & (MFS_ATTR_DIR_NAME | MFS_ATTR_VOLUME_NAME))
{
error_code = MFS_ACCESS_DENIED;
}
else if ((dir_entry.ATTRIBUTE[0] & MFS_ATTR_READ_ONLY) && ((fsflags & MFS_O_ACCMODE) != MFS_O_RDONLY))
{
error_code = MFS_ACCESS_DENIED;
}
else
{
MFS_HANDLE_PTR existing_handle;
/* Check to see if the file is already opened */
existing_handle = MFS_Find_handle_new(drive_ptr, entry_sector, entry_index);
/* Create new handle possibly associating it with the existing one */
handle = MFS_Create_handle(drive_ptr, existing_handle);
if (handle == NULL)
{
error_code = MFS_INSUFFICIENT_MEMORY;
}
/* Fill in data in the directory entry, unless it was associated with an existing handle (i.e. already filled in) */
if (existing_handle == NULL)
{
MFS_dir_entry_from_disk(drive_ptr, handle->DIR_ENTRY, &dir_entry);
handle->DIR_ENTRY->ENTRY_SECTOR = entry_sector;
handle->DIR_ENTRY->ENTRY_INDEX = entry_index;
handle->DIR_ENTRY->DIRTY = 0;
}
}
}
}
The problem is if handle comes back as NULL from MFS_Create_handle, the error_code is set but the NULL handle is still used in the call to MFS_dir_entry_from_disk. This will then generate a bus fault.
I think that putting MFS_dir_entry_from_disk in an else block should solve this:
/* Create new handle possibly associating it with the existing one */
handle = MFS_Create_handle(drive_ptr, existing_handle);
if (handle == NULL)
{
error_code = MFS_INSUFFICIENT_MEMORY;
}
else
{
/* Fill in data in the directory entry, unless it was associated with an existing handle (i.e. already filled in) */
if (existing_handle == NULL)
{
MFS_dir_entry_from_disk(drive_ptr, handle->DIR_ENTRY, &dir_entry);
handle->DIR_ENTRY->ENTRY_SECTOR = entry_sector;
handle->DIR_ENTRY->ENTRY_INDEX = entry_index;
handle->DIR_ENTRY->DIRTY = 0;
}
}
Hope it helps
Hi Adrian,
Thank you for your feedback. I will this to our development team.
Could you please mention the MQX version, IDE and device used?
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------