MCIMX6Q-SDB usb connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCIMX6Q-SDB usb connection

619 Views
jose0225
Contributor II

Hi, I'm newbie in developing MCIMX6Q-SDB.

I'm planning to operating system without specific OS like android or linux.

My question is very simple.

How could I connect this board to PC by usb and make some code and debugging?

And Is windows10 can operate in that condition?

Thank you so much.

Tags (1)
0 Kudos
Reply
1 Reply

424 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

The i.MX is a big processor and it is not common debugging applications without an OS (as Linux and Android BSPs are provided for free).

If you want to implement USB communication without OS, you could try with the SDK package (check the following webpage):

i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale

However, this USB communication is not considered for debugging. If you are looking for a debugging environment (with or without an OS), you could consider ARM DS-5 + DStream environment. You could find additional information below:

http://ds.arm.com/ds-5-community-edition/

http://ds.arm.com/ds-5/debug/dstream/

Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply