MCF 52259 Demokit

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MCF 52259 Demokit

跳至解决方案
4,103 次查看
nms
Contributor I

hi,

 

i am using MCF 52259 Demokit.

i am using MQX sample code from the CD given.

i have downloaded web_hvac_m52259 application.

it is for showing USB flash drive demo,but if i am doing some changes in printf ,that are not getting appeared on hyperterminal.i tried to compile the lib with the help of Application Pdf,but didnt fruitful.

 

Please help.

 

Thanks 

 

0 项奖励
回复
1 解答
2,049 次查看
G_G
Contributor I

After making necessary changes, Press "Make" icon (or you can go to make option from Debug menu) to rebuild the image. Then burn the code again in flash of controller.

 

If problems persists reply back on this blog...... 

在原帖中查看解决方案

0 项奖励
回复
6 回复数
2,049 次查看
nms
Contributor I

hi,

 

I am working on the Sample code given along with CD.(Freescale\Freescale MQX 3.0\demo\web_hvac).This is my application folder. The c code is USB_File.c.

I have added some printf . 

 

After doing make and downloading the code ,the printf changes are  not reflected .

kindly guide me.

 

 nms

0 项奖励
回复
2,049 次查看
DavidS
NXP Employee
NXP Employee

Hi NMS,

The latest version of MQX is 3.2 and there should be a 3.3 next week.

Please re-try with latest FSL MQX and let us know if you still have an issue.

http://www.freescale.com/mqx

The USB drivers have been worked on with each revision as fyi.

Regards,

David

0 项奖励
回复
2,049 次查看
Vijayaragavan
Contributor I

it's urgent.

 

can you please reply as soon as possible?

 

 

0 项奖励
回复
2,049 次查看
Vijayaragavan
Contributor I

Hi

 

i am not clear about how the flash programming is done.are any settings  required?

 

My resources are :

 

1. MCF52259 Demokit

2.JM60 OSBDM - USB

 

i have written a small program that prints "Hello World" on serial.that works fine.

 

if I remove power I mean if i remove usb cable and then once again plug in "Hello World" is not printing on serial.

 

removing usb cable is something like resetting a controller?.

 

i don't understand what is happening?

 

after connecting a usb cable if i press reset button also "Hello World" is not printing on serial.

 

i flashed the program and i reset it is printing "Hello world".

 

Steps i am following are : First time

---------------------------------------------------------------------------

1.connect usb cable to board.Power is given

2.i did flashing.

3.reset the board . Printed "Hello World".

------------------------------------------------------------------------------

 

Steps i am following are : second  time

-----------------------------------------------------------------------------

1.Connect usb cable to board.power is given.

2.reset the board. did not print "Hello World".

 

i am expecting to print "Hello world" at this time. because i already flashed the code.

 

why?

 

 

Thanks

Vijayragavan S

 

 

 

 

 

 

 

 

 

 

 

 

0 项奖励
回复
2,050 次查看
G_G
Contributor I

After making necessary changes, Press "Make" icon (or you can go to make option from Debug menu) to rebuild the image. Then burn the code again in flash of controller.

 

If problems persists reply back on this blog...... 

0 项奖励
回复
2,049 次查看
CarlFST60L
Senior Contributor II
Can you be more specific?
0 项奖励
回复