Low power mode support in MQX 4.2 for Coldfire

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Low power mode support in MQX 4.2 for Coldfire

838件の閲覧回数
ARQuattr
Contributor IV

I'm using Coldfire MCF52254 MCUs on some older hardware, and Kinetis on newer devices, and I have low power mode working for Kinetis, but wanted to add similar functionality for Coldfire.  Back with MQX 3.6, it wasn't supported for Coldfire.  I'm wondering if the recent MQX versions have added support for low power entry and wakeup for Coldfire?

Thanks

Angelo

0 件の賞賛
返信
1 返信

677件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Angelo,

Sorry no specific low power example for your ColdFire device in MQX.

There is AN3236 which reviews low power ColdFire configurations that might be useful.

MQX4.1 does have example of low power for MCF51JF MCU which is a ColdFire V1 core.  So not exactly the same as your V2 core MCU but the structure of the code might enable you to port it to your device.

Regards,

David

0 件の賞賛
返信