Does anyone have a project to build the MQX V4.2.0 USB stack for the Vybrid A5 core using the IAR IDE? In the V4.2.0 distribution there is a USB V2 stack which is supposed to be for the Vybrid processor. In the directory, in the build subdirectory, there is a make file to build the library, but nothing for any of the IDEs. Just wondering if anyone has built the library using IAR tools.
Hi Ken
Please refer to folder Freescale_MQX_4_2\usb_v2\example, there are some demos with IAR
Freescale_MQX_4_2\usb_v2\example\device\msd\mqx\iar\dev_msd_disk_twrvf65gs10_a5
Regards
Daniel