I want a timer that after 3 seconds with out user input the UI is reset. I can start a 3 second timer, but I do not see any way of resetting the timer to 3 seconds. Is there another option to canceling and restarting a timer?
Thanks
MQX 3.6.2
已解决! 转到解答。
Hi Barber,
The lightweight timer is a very simple and limited capability timer module as compared to the full timer operations. The full timer can be setup as a one shot occurence or periodic with a bunch of other capabilities.
Once you start a lightweight timer at whatever periodic rate you want you can cancel it using the _lwtimer_cancel_timer() function call.
Hope this helps.
Regards,
David
Hi Barber,
The lightweight timer is a very simple and limited capability timer module as compared to the full timer operations. The full timer can be setup as a one shot occurence or periodic with a bunch of other capabilities.
Once you start a lightweight timer at whatever periodic rate you want you can cancel it using the _lwtimer_cancel_timer() function call.
Hope this helps.
Regards,
David