K66 on MQX 4.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K66 on MQX 4.2

1,290件の閲覧回数
arnogir
Senior Contributor II

Hello,

I Have already designed some application on K60F150, K70F150, with MQX 4.2 and PEG.

For a new application, we need a µC with 2MB Flash and 256KB of RAM to avoid use a sqm4 K70 bord to reduce the cost.

Is the K66F180 is supported by MQX 4.2? Because into it, there are repository for K60 ,64, 65 and 70 but not for K66.

K65 seems to be the 1MB flash supported, not the 2MB.

Do you think I can use the K65f180 and just modify the linker file to extend flash from 1MB to 2MB?

Thank

0 件の賞賛
返信
2 返答(返信)

1,102件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi  Arnaud:

K66 Board is supported in MQX v5 , it is under low-cost commercial license terms. Please check below link for more details.

MQX™ v5 Software Solutions|NXP 

If you want to port from K65f180, it is also possible, please read the porting guide in the MQX 4.2 installation folder.  Just modify the linker file is not enough.

Regards

Daniel

0 件の賞賛
返信

1,102件の閲覧回数
arnogir
Senior Contributor II

Ok Thank for your background.

0 件の賞賛
返信