Hi Carlos,
Thank you for replying. Please see below for the linker directive file that I have modified to meet my needs. I also included the kinetis.h file, as I had to make some modifications to the __HEAP_START and __HEAP_END defines because of the non-standard configuration. How much heap is typically needed for a program running on the Kinetis board? It seems that the application I am running requires a great deal, as I have many classes I am newing at start-up.
----------------------------------------Linker Directive File ---------------------------
/* Entry Point */
ENTRY(Reset_Handler)
HEAP_SIZE = DEFINED(__heap_size__) ? __heap_size__ : 0x00;
STACK_SIZE = DEFINED(__stack_size__) ? __stack_size__ : 0x0400;
/* Specify the memory areas */
MEMORY {
m_interrupts (RX) : ORIGIN = 0x00000000, LENGTH = 0x00000400
m_flash_config (RX) : ORIGIN = 0x00000400, LENGTH = 0x00000010
m_interrupts_ram (RW) : ORIGIN = 0x1FFF0000, LENGTH = 0x00000400
m_text (RX) : ORIGIN = 0x00000410, LENGTH = 0x000FFBF0
m_data (RW) : ORIGIN = 0x1FFF0400, LENGTH = 0x0000FC00
m_data_2 (RW) : ORIGIN = 0x20000000, LENGTH = 0x00030000
}
/* Define output sections */
SECTIONS
{
/* The startup code goes first into INTERNAL_FLASH */
.interrupts :
{
__VECTOR_TABLE = .;
. = ALIGN(4);
KEEP(*(.isr_vector)) /* Startup code */
. = ALIGN(4);
} > m_interrupts
__VECTOR_RAM = ORIGIN(m_interrupts_ram);
.flash_config :
{
. = ALIGN(4);
KEEP(*(.FlashConfig)) /* Flash Configuration Field (FCF) */
. = ALIGN(4);
} > m_flash_config
/* The program code and other data goes into INTERNAL_FLASH */
.text :
{
. = ALIGN(4);
*(.text) /* .text sections (code) */
*(.text*) /* .text* sections (code) */
*(.rodata) /* .rodata sections (constants, strings, etc.) */
*(.rodata*) /* .rodata* sections (constants, strings, etc.) */
*(.glue_7) /* glue arm to thumb code */
*(.glue_7t) /* glue thumb to arm code */
*(.eh_frame)
KEEP (*(.init))
KEEP (*(.fini))
. = ALIGN(4);
} > m_text
.ARM.extab :
{
*(.ARM.extab* .gnu.linkonce.armextab.*)
} > m_text
.ARM :
{
__exidx_start = .;
*(.ARM.exidx*)
__exidx_end = .;
} > m_text
.ctors :
{
__CTOR_LIST__ = .;
/* gcc uses crtbegin.o to find the start of
the constructors, so we make sure it is
first. Because this is a wildcard, it
doesn't matter if the user does not
actually link against crtbegin.o; the
linker won't look for a file to match a
wildcard. The wildcard also means that it
doesn't matter which directory crtbegin.o
is in. */
KEEP (*crtbegin.o(.ctors))
KEEP (*crtbegin?.o(.ctors))
/* We don't want to include the .ctor section from
from the crtend.o file until after the sorted ctors.
The .ctor section from the crtend file contains the
end of ctors marker and it must be last */
KEEP (*(EXCLUDE_FILE(*crtend?.o *crtend.o) .ctors))
KEEP (*(SORT(.ctors.*)))
KEEP (*(.ctors))
__CTOR_END__ = .;
} > m_text
.dtors :
{
__DTOR_LIST__ = .;
KEEP (*crtbegin.o(.dtors))
KEEP (*crtbegin?.o(.dtors))
KEEP (*(EXCLUDE_FILE(*crtend?.o *crtend.o) .dtors))
KEEP (*(SORT(.dtors.*)))
KEEP (*(.dtors))
__DTOR_END__ = .;
} > m_text
.preinit_array :
{
PROVIDE_HIDDEN (__preinit_array_start = .);
KEEP (*(.preinit_array*))
PROVIDE_HIDDEN (__preinit_array_end = .);
} > m_text
.init_array :
{
PROVIDE_HIDDEN (__init_array_start = .);
KEEP (*(SORT(.init_array.*)))
KEEP (*(.init_array*))
PROVIDE_HIDDEN (__init_array_end = .);
} > m_text
.fini_array :
{
PROVIDE_HIDDEN (__fini_array_start = .);
KEEP (*(SORT(.fini_array.*)))
KEEP (*(.fini_array*))
PROVIDE_HIDDEN (__fini_array_end = .);
} > m_text
__etext = .; /* define a global symbol at end of code */
__DATA_ROM = .; /* Symbol is used by startup for data initialization */
.data : AT(__DATA_ROM)
{
. = ALIGN(4);
__DATA_RAM = .;
__data_start__ = .; /* create a global symbol at data start */
*(.data) /* .data sections */
*(.data*) /* .data* sections */
KEEP(*(.jcr*))
. = ALIGN(4);
__data_end__ = .; /* define a global symbol at data end */
} > m_data_2
/* Symbol is used by startup for data initialization */
__DATA_END = __DATA_ROM + (__data_end__ - __data_start__);
__m_interrupts_ram_ROMStart = __DATA_ROM + SIZEOF(.data);
.m_interrupts_ram : AT(__m_interrupts_ram_ROMStart)
{
. = ALIGN(4);
__m_interrupts_ram_RAMStart = .;
*(.m_interrupts_ram) /* This is an User defined section */
. += 0x0400;
__m_interrupts_ram_RAMEnd = .;
. = ALIGN(4);
} > m_interrupts_ram
__m_interrupts_ram_ROMSize = __m_interrupts_ram_RAMEnd - __m_interrupts_ram_RAMStart;
__RAM_VECTOR_TABLE_SIZE_BYTES = __m_interrupts_ram_RAMEnd - __m_interrupts_ram_RAMStart;
__m_data_2_ROMStart = __m_interrupts_ram_ROMStart + SIZEOF(.m_interrupts_ram);
.m_data_2 : AT(__m_data_2_ROMStart)
{
. = ALIGN(4);
__m_data_2_RAMStart = .;
*(.m_data_2) /* This is an User defined section */
__m_data_2_RAMEnd = .;
. = ALIGN(4);
} > m_data_2
__m_data_2_ROMSize = __m_data_2_RAMEnd - __m_data_2_RAMStart;
/* Uninitialized data section */
.bss :
{
/* This is used by the startup in order to initialize the .bss section */
. = ALIGN(4);
__START_BSS = .;
__bss_start__ = .;
*(.bss)
*(.bss*)
*(COMMON)
. = ALIGN(4);
__bss_end__ = .;
__END_BSS = .;
} > m_data
.heap :
{
. = ALIGN(8);
__end__ = .;
PROVIDE(end = .);
__HeapBase = .;
. += HEAP_SIZE;
__HeapLimit = .;
} > m_data_2
.stack :
{
. = ALIGN(8);
. += STACK_SIZE;
} > m_data
__StackTop = ORIGIN(m_data) + LENGTH(m_data);
__StackLimit = __StackTop - STACK_SIZE;
__heap_start = __data_end__ ;
__heap_end = __data_end__ + HEAP_SIZE;
PROVIDE(__stack = __StackTop);
.ARM.attributes 0 : { *(.ARM.attributes) }
}
---------------------------------------- Kinetis File ---------------------------
* See license agreement file for full license terms including other
* restrictions.
*****************************************************************************
*
* Comments:
*
* This file contains the type definitions for the Kinetis microcontrollers.
*
*
*END************************************************************************/
#ifndef __kinetis_h__
#define __kinetis_h__
#ifndef __ASM__
#include <mqx.h>
/* Include FSK device registers from Platform SDK */
#include "fsl_device_registers.h"
#include "nvic.h"
#include "kinetis_mpu.h"
#endif /* __ASM__ */
#ifdef __cplusplus
extern "C" {
#endif
/*
*******************************************************************************
**
** LINKER SYMBOLS ACCESS
**
*******************************************************************************
*/
/* Addresses for VECTOR_TABLE and VECTOR_RAM come from the linker file */
#if defined(__CC_ARM) /* Keil MDK */
extern uint32_t Image$$ARM_LIB_HEAP$$Base[];
extern uint32_t Image$$ARM_LIB_STACK$$ZI$$Base[];
extern uint32_t Image$$VECTOR_ROM$$Base[];
extern uint32_t Image$$VECTOR_RAM$$Base[];
#define __VECTOR_TABLE Image$$VECTOR_ROM$$Base
#define __VECTOR_RAM Image$$VECTOR_RAM$$Base
#define __HEAP_START Image$$ARM_LIB_HEAP$$Base
#define __HEAP_END Image$$ARM_LIB_STACK$$ZI$$Base /* Segment is defined in opposite way (from higher address to lower) than usually!!! */
#elif defined(__ICCARM__) /* IAR */
#pragma section = "ZI"
#define __ZI_END (__section_end("ZI"))
#pragma section = "RW"
#define __RW_END (__section_end("RW"))
#pragma section = "HEAP"
#define __HEAP_START (__section_begin("HEAP"))
#pragma section = "CSTACK"
#define __HEAP_END (__section_begin("CSTACK"))
extern uint32_t __VECTOR_TABLE[NUMBER_OF_INT_VECTORS * sizeof(uint32_t)];
extern uint32_t __VECTOR_RAM[NUMBER_OF_INT_VECTORS * sizeof(uint32_t)];
#elif defined(__GNUC__) /* GCC */
//extern uint32_t __bss_end__[];
//extern uint32_t __StackLimit[];
extern uint32_t __heap_start[];
extern uint32_t __heap_end[];
#define __HEAP_START __heap_start
#define __HEAP_END __heap_end
extern uint32_t __VECTOR_TABLE[NUMBER_OF_INT_VECTORS * sizeof(uint32_t)];
extern uint32_t __VECTOR_RAM[NUMBER_OF_INT_VECTORS * sizeof(uint32_t)];
#else
#error Unsupported tool
#endif
<Extra lines removed>