K64 Freedom _task_delay() not Working Properly

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K64 Freedom _task_delay() not Working Properly

3,857 次查看
razed11
Contributor V

The BSP documentations says: ...Alternatively, the bsp_cm.c can be modified manually without PEx.

It then goes on to say nothing more about it. A document about changing clock settings is referenced but I can't find it anywhere.

I'd like to understand how the clocks are configured. I'm wondering how SysTick is configured because on the K64 Freedom when I call _task_delay(10) I'm getting 150 ms instead.

标记 (2)
0 项奖励
回复
2 回复数

3,713 次查看
soledad
NXP Employee
NXP Employee

Hi Kenny,

I am attaching this document, this document is located at the path: C:\Freescale\Freescale_MQX_4_1\doc\tools\cw


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,713 次查看
razed11
Contributor V

Thanks! A little bias towards the CW people I see. Let me see if this helps.

0 项奖励
回复