K60 Hight speed with MQX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

K60 Hight speed with MQX

跳至解决方案
1,432 次查看
Kuroro
Contributor II

Hi

 

i want to know if the last version of MQX support the USB HS mode on the K60 (witch is USB HS compliant).

And if this feature is supported how to configure MQX to take advantage of it ?

 

Thank's

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,068 次查看
JuroV
NXP Employee
NXP Employee

USB module in K60 is not USB HS compliant.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,068 次查看
technologyguru
Contributor I

I was recently informed by Freescale that the 100Mhz part does not have USB support but the 120MHZ parts do. They are not available until Nov 2011 and that includes MQX suppport. Despite the hype last year of the parts availability by July of 2011 these parts will not see the light of day for months. If you need HS USB try the Atmel 91Sam 3U parts that also have the UTMI tranceiver built in. However it is a Cortex M-3 part unlike the K60 which is a M-4 part. I had to design the Freescale out of a a new circuit and had to replace it with an alternative. Hopefully, Freescale will regain its reputation.

1,069 次查看
JuroV
NXP Employee
NXP Employee

USB module in K60 is not USB HS compliant.

0 项奖励
回复