K60 Hight speed with MQX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K60 Hight speed with MQX

Jump to solution
1,407 Views
Kuroro
Contributor II

Hi

 

i want to know if the last version of MQX support the USB HS mode on the K60 (witch is USB HS compliant).

And if this feature is supported how to configure MQX to take advantage of it ?

 

Thank's

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,043 Views
JuroV
NXP Employee
NXP Employee

USB module in K60 is not USB HS compliant.

View solution in original post

0 Kudos
Reply
2 Replies
1,043 Views
technologyguru
Contributor I

I was recently informed by Freescale that the 100Mhz part does not have USB support but the 120MHZ parts do. They are not available until Nov 2011 and that includes MQX suppport. Despite the hype last year of the parts availability by July of 2011 these parts will not see the light of day for months. If you need HS USB try the Atmel 91Sam 3U parts that also have the UTMI tranceiver built in. However it is a Cortex M-3 part unlike the K60 which is a M-4 part. I had to design the Freescale out of a a new circuit and had to replace it with an alternative. Hopefully, Freescale will regain its reputation.

1,044 Views
JuroV
NXP Employee
NXP Employee

USB module in K60 is not USB HS compliant.

0 Kudos
Reply