We are using the MQX MFS system and USB driver and need the correct date and time on the file systems. We would like to set the time in the RTC module and retrieve it again on subsequent boots so that the file system times are correct. Can anyone suggest a best practice for setting the time for using the RTC please.
I noticed that when I create a new file, it has a created date of 01-Jan-80, but the correct date in the 'Modified' column. Is there a way to cause MQX or the MFS system to place the correct date on both aspects of the file system. I am using the _time_set(&time_struct) mqx call.
Thanks
Robert
解決済! 解決策の投稿を見る。
Hi David
That looks exactly like what we need.
I went to download mqx 4.0.2 but the download link says that it is an evaluation download.... can you explain what that means please?
Do I download the eval copy, then patch it up to 4.0.2.1 then to 4.0.2.2? I wouldn't like to build an eval into the project to have it timeout or corrupt at some point in the future.
I would have marked your answer as a solved solution but I looked all over the page for some button or method to do so but couldn't find one. Sorry.
Thanks for the help and responding
Robert
Hi Robert,
The MQX4_0_2/docs/mqx/MQXIOUG.pdf has following:
Chapter 15 RTC Driver
15.1 Overview
This section describes the Real Time Clock (RTC) driver that accompanies the MQX release. This driver
is a common interface for both RTC and Independent Real Time Clock (IRTC) peripheral modules.
The RTC driver implements custom API and does not follow the standard driver interface (I/O
Subsystem).
Lots of information there.
We also have example in the MQX4.0.2 using RTC:
C:\Freescale\Freescale_MQX_4_0_2\mqx\examples\rtc
I think this will help you but I haven't played with it yet.
Regards,
David
Hi David
That looks exactly like what we need.
I went to download mqx 4.0.2 but the download link says that it is an evaluation download.... can you explain what that means please?
Do I download the eval copy, then patch it up to 4.0.2.1 then to 4.0.2.2? I wouldn't like to build an eval into the project to have it timeout or corrupt at some point in the future.
I would have marked your answer as a solved solution but I looked all over the page for some button or method to do so but couldn't find one. Sorry.
Thanks for the help and responding
Robert
Hi Robert, no idea why the mqx4.0.2 download link is named that way. Just ignore, download, and do same with both patches.
I'll mention our web people to fix.
Happy Holidays,
David
Sent from my iPhone