Issue with ftp in lab tutorial for TWR-MCF5225X

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issue with ftp in lab tutorial for TWR-MCF5225X

785 次查看
MWMinor
Contributor V

Hi - I am finding some difficulty running the MCF5225X - lab tutorial #3. The telnet operation works fine, but after configuring the HVAC.h file for the ftp portion, I get stuck when I try to login;

>ftp 169.254.3.3 responds with a request for username. The guide says to press return and you should be logged in but the program seems to insist on a username, and if you try to use one it asks for a password.

Has anyone else seen this problem...?

Ken

0 项奖励
回复
2 回复数

678 次查看
soledad
NXP Employee
NXP Employee

Hello Ken,

The ftp problems usually appear when is not enough memory available. Could you please share more information about your project?? Which MQX version are you using??

Regards

Sol

0 项奖励
回复

678 次查看
Wlodek_D_
Senior Contributor II

Dear Ken Armitage,

Thank you for your post, however please consider moving it to the right community place for better visibility.

For details please see general advice https://community.freescale.com/docs/DOC-99909

Thank you for using Freescale Community.

Regards,

Wlodek_D.

0 项奖励
回复