Issue with ftp in lab tutorial for TWR-MCF5225X

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue with ftp in lab tutorial for TWR-MCF5225X

758件の閲覧回数
MWMinor
Contributor V

Hi - I am finding some difficulty running the MCF5225X - lab tutorial #3. The telnet operation works fine, but after configuring the HVAC.h file for the ftp portion, I get stuck when I try to login;

>ftp 169.254.3.3 responds with a request for username. The guide says to press return and you should be logged in but the program seems to insist on a username, and if you try to use one it asks for a password.

Has anyone else seen this problem...?

Ken

0 件の賞賛
返信
2 返答(返信)

651件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello Ken,

The ftp problems usually appear when is not enough memory available. Could you please share more information about your project?? Which MQX version are you using??

Regards

Sol

0 件の賞賛
返信

651件の閲覧回数
Wlodek_D_
Senior Contributor II

Dear Ken Armitage,

Thank you for your post, however please consider moving it to the right community place for better visibility.

For details please see general advice https://community.freescale.com/docs/DOC-99909

Thank you for using Freescale Community.

Regards,

Wlodek_D.

0 件の賞賛
返信