Is there any way to write to sdcard using the dma?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there any way to write to sdcard using the dma?

14,496件の閲覧回数
naftalir
Contributor III

Hi all,

 

if anyone have any exmample of fast writing to sdcard, with dma and/or with 4bit bandswidth, plz send me an source code..

 

Thank you so much!

Naftali. 

ラベル(1)
タグ(1)
0 件の賞賛
返信
4 返答(返信)

1,011件の閲覧回数
naftalir
Contributor III

Can you be a little bit more specific on when the answers will be :smileyhappy:?

Thank you....

0 件の賞賛
返信

1,011件の閲覧回数
Monica
Senior Contributor III

Hey everyone!

Answers will arrive very soon!

Thanks for being all so patient!!!

Regards,

Monica

0 件の賞賛
返信

1,011件の閲覧回数
jonny
Contributor I

Did you have any luck with this?

0 件の賞賛
返信

1,011件の閲覧回数
naftalir
Contributor III

Nothing yet.... did you?

0 件の賞賛
返信