Is there an MQX IAR package for the 5272 coldfire

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there an MQX IAR package for the 5272 coldfire

311 Views
jschimpf
Contributor I

I have an old MQX 2.4 version but it is not set up for IAR, is there an IAR version of MQX (newer is OK) for the 5272 ?

Thanks,

     --jschimpf

0 Kudos
1 Reply

237 Views
soledad
NXP Employee
NXP Employee

Hello Jim,

MQX2.4 was not developed by Freescale, this version was developed by our partner Embedded Access. Freescale porvides MQX for free but it does not support MCF5272. If you want a special porting you may contact Embedded Access at www.embeddedaccess.com or purchase Freescale level 2 support at www.freescale.com/mqx/support


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos