Is there a PE tutorial for MQX? All the examples I have found are non mqx. One of the questions I have is under the MQX directory is see
C:\Freescale\Freescale_MQX_4_0\demo\pe_demo
C:\Freescale\Freescale_MQX_4_0\mqx\examples
C:\Freescale\Freescale_MQX_4_0\usb\host
Which of these three examples do I use for a PE based project that user MQX and can act as a USB host.
Thanks
I also looked in the PE forums but did not see a good answer so I posted here.
已解决! 转到解答。
Hi Dale,
Yes, there is a tutorial for using Processor Expert (PEx) with MQX. It’s included in the documentation installed with MQX. You will find it at \Freescale_MQX_4_0\doc\tools\cw\FSL_MQX_in_CW_10_x.pdf
The pe_demo is a demo application for using PEx in your BSP, and is discussed in the tutorial above.
Hi Dale,
Yes, there is a tutorial for using Processor Expert (PEx) with MQX. It’s included in the documentation installed with MQX. You will find it at \Freescale_MQX_4_0\doc\tools\cw\FSL_MQX_in_CW_10_x.pdf
The pe_demo is a demo application for using PEx in your BSP, and is discussed in the tutorial above.